2017-12-24 5:29 PM
In STM32F4's HAL code for function 'HAL_TIM_OnePulse_Start':
/**
* @brief Starts the TIM One Pulse signal generation.
* @param htim pointer to a TIM_HandleTypeDef structure that contains
* the configuration information for TIM module.
* @param OutputChannel TIM Channels to be enabled.
* This parameter can be one of the following values:
* @arg TIM_CHANNEL_1: TIM Channel 1 selected
* @arg TIM_CHANNEL_2: TIM Channel 2 selected
* @retval HAL status
*/
HAL_StatusTypeDef
HAL_TIM_OnePulse_Start
(TIM_HandleTypeDef
*
htim,
uint32_t
OutputChannel)
{
/* Prevent unused argument(s) compilation warning */
UNUSED
(OutputChannel);
/* Enable the Capture compare and the Input Capture channels
(in the OPM Mode the two possible channels that can be used are TIM_CHANNEL_1 and TIM_CHANNEL_2)
if TIM_CHANNEL_1 is used as output, the TIM_CHANNEL_2 will be used as input and
if TIM_CHANNEL_1 is used as input, the TIM_CHANNEL_2 will be used as output
in all combinations, the TIM_CHANNEL_1 and TIM_CHANNEL_2 should be enabled together
No need to enable the counter, it's enabled automatically by hardware
(the counter starts in response to a stimulus and generate a pulse */
TIM_CCxChannelCmd
(htim->
Instance
, TIM_CHANNEL_1, TIM_CCx_ENABLE);
TIM_CCxChannelCmd
(htim->
Instance
, TIM_CHANNEL_2, TIM_CCx_ENABLE);
if
(
IS_TIM_ADVANCED_INSTANCE
(htim->
Instance
)
!=
RESET)
{
/* Enable the main output */
__HAL_TIM_MOE_ENABLE
(htim);
}
/* Return function status */
return
HAL_OK;
}
It seems only CH1 and CH2 is used, does this mean only CH1 or CH2 can be used in one-pulse mode?
#one-pulse-mode2017-12-25 9:33 AM
One-pulse is a mode of the counter, i.e. that the counter disables itself upon update event (i.e. overflows). There's nothing capture/compare-specific in it, i.e. it's relevant to all channels in the same way.
JW
2017-12-25 10:10 PM
You mean all channels of the timer will support this mode? But why the HAL code only use
TIM_CHANNEL_1 and
TIM_CHANNEL_2?
2018-01-17 3:35 PM
Because this is not what OPM (i.e. mode enabled by TIMx_CR1.OPM) is about.
This function is part of a suite fulfilling one single, complex and quite useless task - turning the timer into a one-shot. This is Cube ad absurdum: this ought to be an example, not part of a 'library'.
Btw. even for this task, the functions are unnecessarily crippled: while the inputs indeed can be only of channels 1 and 2 (as trigger source to slave-mode controller), any channel could be as output.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.