2024-07-18 4:39 AM - last edited on 2024-07-18 4:43 AM by mƎALLEm
I am trying to interface CAN communication in loopback mode in STM32F469I DISCO but it is not working.
Solved! Go to Solution.
2024-07-18 4:58 AM - edited 2024-07-24 1:01 AM
There is no CAN examples available for STM32F469I DISCO board but you can inspire from the example provided in the STM32CubeF4 in github from this link for STM32469I_EVAL board (the same microcontroller, but you need to check the RCC and the CAN GPIO pins configurations):
But you didn't share your code to look at it.
Two questions:
Did you enable and configure correctly the filters.
Did you configure the internal pull-up resistor for CAN_Rx pin ? if not it needs to be configured.
2024-07-18 4:42 AM
Hello @jrupesh90_ and welcome to the community.
You need to describe what kind of issue you are facing.
You can refer to this link on how to post a thread.
You need to share your project including the ioc file.
2024-07-18 4:53 AM
I am trying to interface CAN in loopback mode in STM32F469I DISCO board but my code is not working. Can you provide me some code snippets with respect to board.
2024-07-18 4:58 AM - edited 2024-07-24 1:01 AM
There is no CAN examples available for STM32F469I DISCO board but you can inspire from the example provided in the STM32CubeF4 in github from this link for STM32469I_EVAL board (the same microcontroller, but you need to check the RCC and the CAN GPIO pins configurations):
But you didn't share your code to look at it.
Two questions:
Did you enable and configure correctly the filters.
Did you configure the internal pull-up resistor for CAN_Rx pin ? if not it needs to be configured.
2024-07-24 1:01 AM
Hello @jrupesh90_ ,
Could you please give a status of this thread and tell if you solved your issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.