2013-05-29 3:42 AM
can i trigger sdadc1 with OC2 of tim19 ,and trigger sdadc2 with OC3 of tim19? then sdadc1 trigger dma2 in channel3,sdadc2 trigger dma2 in channel4.can stm32f373 do this ??
#stm32f3732013-05-29 4:50 AM
Signs point to yes.
2013-05-29 5:40 AM
thanks for your reply.and another question(ha ha):
can i trigger sdadc1 & sdadc2 with oc2 of tim19 at the same time?2013-05-29 6:39 AM
The documentation suggests you can't, but I'm not sure this is a big problem because the channels can be programmed the same (generate same edges, at same time), and are synchronous, and don't need to reach a physical pin. TIM19 has to run at your sample rate anyway, so it's not as if you really free up any resources.
DMA is just a side-effect of the conversion completing.2013-05-29 7:01 AM
thanks for your reply.yes,i want to sample sdadc1 & sdadc2 synchronously,and save the data in different array.how can i do to make it? I don't want to use sdadc in simultaneous mode.because the dma does not have ping-pong mode.
''The documentation suggests you can't'', which document?2013-05-29 7:28 AM
I was reviewing the RM0313
I built similar code on all the other STM32 series parts by going through the docs, and example code in the libraries, and cut-n-pasting the pieces I could, and coding whatever I needed to stitch them together. All of the DMA units on these parts should have a circular mode, with HT (Half Transfer) and TC (Transfer Complete) interrupts, and are perfectly adept at doing ping-pong operation to two halves of a linear buffer. Some of the parts offer the ability to handle two fragmented buffers, although I think that just adds more complexity than is required. Not for the F3, but illustrative[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/stm32f207%20ADC%2BTIMER%2BDMA%20%20Poor%20Peripheral%20Library%20Examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=128]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2Fstm32f207%20ADC%2BTIMER%2BDMA%20%20Poor%20Peripheral%20Library%20Examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1282013-05-29 6:14 PM
thanks for reply
which page of RM0313 suggests me can't? page 213 says''This timing trigger control is capable of triggering simultaneous conversion or inserting a programmable delay between the SDADCS''We’re moving the ST Community to a new platform to give you a better and more reliable community experience.