2019-01-04 12:05 PM
I am using the STM32H743 on STM32H743I-EVAL board.
Is it possible to synchronize ADC acquisitions with the SAI block? The goal here is to acquire audio ADC samples using DMA, block process, and transmit out to a DAC over SAI using DMA. The STM32 is the master generating SAI clocks. In order to keep system synced I need to acquire ADC samples at the same frequency as the SAI frame sync clock.
From the reference manual, there are a few output signals from the SAI block that would be ideal candidates, "sai_sync_out_sck" or "sai_sync_out_fs". Is it possible to trigger the ADC, or trigger a timer which in turn triggers ADC, with these internal signals?
Alternatively, is it possible to use a timer as the clock source to the SAI block?
2019-01-04 1:39 PM
I don't use the 'H7, but from the Interconnect chapter it appears that the SAIx_FS_A/B signals are connected to ETR inputs of timers.
JW
2019-01-07 7:32 AM
Thank you for bringing this to my attention JW. I will implement this and see how it works. The trade-off with this approach is that the timer has a clocked ERT input and is therefore asynchronous to the SAI FS signal. This will introduce ADC sampling jitter.
I suppose I could run the entire system at PLL settings that are audio sample rate friendly. I don't want to do this because I will not be running at max speed of 400MHz, which is the primary reason I'm using the part.
2019-01-08 5:07 AM
I'd say there will always be some synchronizers in the way; I believe that not only in the timer, but there may be some at the ADC's front-end, too.
Unfortunately, ST is not famous for providing excessive data on these minor but important design details.
You may want to have a look at the LPTIMs, too; they ought to be asynchronous (to some extent).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.