2023-10-16 5:49 AM
I have a Nucleo-l432kc board that I actually fried by accident touching one of the pins with my power supply probes while they shared the same ground during a risky test of mine
anyway the problem now is I can't find a replacement at the moment in my region and a shipment of Aliexpress would take some time I have some Blackpills and Clone stlinks lying around but using those clones have no mass storage or Virtual com port feature
My Question is can I use the stlink on my fried board somehow ? I think the stlink circuitry itself is working fine since the mass storage and the openocd commands are working fine except that the cpu won't respond to uploading any code
Solved! Go to Solution.
2023-10-16 6:40 AM
In principle, you could use an ST-LINK - however, this requires the separation of some tracks, because unlike NUCLEO-64, for example, there is no space for solder bridges. You would have to disconnect and connect with the external ST-LINK:
In addition, you may have to put X1, C12, C13 and SB5/SB7 and to remove SB4 if you need a stable clock, as MCO from the built-in ST-LINK will probably also no longer work.
All in all, quite complex - but perhaps feasible. For more details, I recommend studying the schematics of this NUCLEO-32 (MB1180).
Good luck!
/Peter
2023-10-16 6:40 AM
In principle, you could use an ST-LINK - however, this requires the separation of some tracks, because unlike NUCLEO-64, for example, there is no space for solder bridges. You would have to disconnect and connect with the external ST-LINK:
In addition, you may have to put X1, C12, C13 and SB5/SB7 and to remove SB4 if you need a stable clock, as MCO from the built-in ST-LINK will probably also no longer work.
All in all, quite complex - but perhaps feasible. For more details, I recommend studying the schematics of this NUCLEO-32 (MB1180).
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.