2019-10-31 8:06 AM
2019-10-31 9:51 AM
You can call into the ROM, the processor can execute any arbitrary code you point it too.
You can remap memory, get the Reference Manual, search MEMRMP
2019-11-06 6:47 AM
Thank you for your answer.
I've tried this with this code. But it doesnt work. Do you see any mistakes?
/**
* Function to perform jump to system memory boot from user application
*
* Call function when you want to jump to system memory
*/
void JumpToBootloader(void) {
void (*SysMemBootJump)(void);
/**
* Step: Set system memory address.
*
* For STM32F429, system memory is on 0x1FFF 0000
* For other families, check AN2606 document table 110 with descriptions of memory addresses
*/
volatile uint32_t addr = 0x1FFF0000;
/**
* Step: Disable RCC, set it to default (after reset) settings
* Internal clock, no PLL, etc.
*/
HAL_RCC_DeInit();
/**
* Step: Disable systick timer and reset it to default values
*/
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
/**
* Step: Disable all interrupts
*/
__disable_irq();
/**
* Step: Remap system memory to address 0x0000 0000 in address space
* For each family registers may be different.
* Check reference manual for each family.
*
* For STM32F4xx, MEMRMP register in SYSCFG is used (bits[1:0])
* For STM32F0xx, CFGR1 register in SYSCFG is used (bits[1:0])
* For others, check family reference manual
*/
//Remap by hand... {
//SYSCFG->MEMRMP = 0x01;
//} ...or if you use HAL drivers
__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH(); //Call HAL macro to do this for you
/**
* Step: Set jump memory location for system memory
* Use address with 4 bytes offset which specifies jump location where program starts
*/
SysMemBootJump = (void (*)(void)) (*((uint32_t *)(addr + 4)));
/**
* Step: Set main stack pointer.
* This step must be done last otherwise local variables in this function
* don't have proper value since stack pointer is located on different position
*
* Set direct address location which specifies stack pointer in SRAM location
*/
__set_MSP(*(uint32_t *)addr);
/**
* Step: Actually call our function to jump to set location
* This will start system memory execution
*/
SysMemBootJump();
/**
* Step: Connect USB<->UART converter to dedicated USART pins and test
* and test with bootloader works with STM32 Flash Loader Demonstrator software
*/
}
2019-11-06 10:11 AM
Is the SYSCFG clock enabled, does someone of the other side enable the CPU IRQ?
Used this method on the F205/F405 for a decade or more
Reset_Handler PROC
EXPORT Reset_Handler [WEAK]
IMPORT SystemInit
IMPORT __main
LDR R0, =0x2001FFFC
LDR R1, =0xBEEFBEEF
LDR R2, [R0, #0]
CMP R1, R2
BNE NotDFuse
STR R0, [R0, #0] ; Invalidate
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
LDR R0, =0x1FFF0000 ; ROM BASE
LDR SP,[R0, #0]
LDR R0,[R0, #4]
BX R0
NotDFuse
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ENDP ; sourcer32@gmail.com
2019-11-06 10:15 AM
The F427 may be a more complex beast with the ROM checking banking and bootable FLASH code. Use a Debugger, and determine if the ROM just bounces back control to your Reset Handler. In which case you'll probably want to implement your own loader to facilitate USB/DFU or USART update methods.
2019-11-08 9:47 AM
Hi Clive
I think, I dont understan what exactly is to do. I'm new to MCU.
I read many posts and also this one.
"Mixing up random ideas you copy and paste is not programming. Read the manuals and understand what you are doing."
I really want to understand how its works and what is to do.
Can yoe please help me?
What I know or think to know:
Is that correct or is smth. missing?
Just crarify the thing on a hingher level and the go step by step deeper.
I hope you can help me to go trough the things and finally to reach tje goal.
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.