2023-11-01 2:43 AM
Hi All,
I have a program that is supposed to transfer data from the integrated ADC on STM32H723 to the D1 RAM. I am using DMA for this, but the problem is that the DMA buffer is limited to 64KB, where I need around 200-250 KB buffer size. Here I am thinking about using DMA as a circular buffer, where I want
void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc){
//Trigger MDMA block transfer
}
//Called when buffer is completely filled
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){
//Trigger MDMA block transfer
}to trigger a block transfer from half the DMA buffer to the MDMA buffer (to one linked list node), or simply using a flag. However is this possible? Can I link a flag or something else to trigger a MDMA linked list block transfer? The linked list will consist of 8 nodes of half the DMA buffer size, so that the functionality will be like a circular buffer of ~200 KB.
If someone have done something similar or have an idea how to solve this, I would really appreciate it!
Best regards
Solved! Go to Solution.
2023-11-09 4:54 AM
After a week of headscratching I have made it work! For those who struggle with MDMA here is a code using a circular buffered linked list. The SRC_Buffer can simulate an ADC who have filled one half of a buffer using DMA. Then the DMA callback funcitons can trigger the MDMA to transfer the data to bigger buffers fast.
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define SRC_BUF_SIZE 50000 //65472
#define SRC_BUF_HALF_SIZE 25000 //32736
#define DST_BUF_SIZE 25000 //32736
#define XFR_BUF_SIZE 25000 //32736
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
MDMA_HandleTypeDef hmdma_mdma_channel0_sw_0;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_1;
/* USER CODE BEGIN PV */
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_2;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_3;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_4;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_5;
uint8_t SRC_Buf0[SRC_BUF_SIZE];
uint8_t* SRC_Buf1 = &SRC_Buf0[SRC_BUF_HALF_SIZE];
uint8_t DST_Buf0[DST_BUF_SIZE];
uint8_t DST_Buf1[DST_BUF_SIZE];
uint8_t DST_Buf2[DST_BUF_SIZE];
uint8_t DST_Buf3[DST_BUF_SIZE];
uint8_t DST_Buf4[DST_BUF_SIZE];
uint8_t DST_Buf5[DST_BUF_SIZE];
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Initialize(void);
static void MPU_Config(void);
static void MX_MDMA_Init(void);
/* USER CODE BEGIN PFP */
static void MDMA_TransferCompleteCallback(MDMA_HandleTypeDef *hmdma);
static void MDMA_TransferErrorCallback(MDMA_HandleTypeDef *hmdma);
static void MDMA_TransferBlockCompleteCallback(MDMA_HandleTypeDef *hmdma);
//static void MDMA_TransferBufferCompleteCallback(MDMA_HandleTypeDef *hmdma);
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
unsigned int j = 0;
for(unsigned int i = 0; i < SRC_BUF_SIZE; i++){
SRC_Buf0[i] = j;
j++;
if(j >= 256){
j = 0;
}
}
for(unsigned int i = 0; i < DST_BUF_SIZE; i++){
DST_Buf0[i] = 0;
DST_Buf1[i] = 0;
DST_Buf2[i] = 0;
DST_Buf3[i] = 0;
DST_Buf4[i] = 0;
DST_Buf5[i] = 0;
}
__NOP();
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_MDMA_Init();
/* USER CODE BEGIN 2 */
if (HAL_MDMA_Start_IT(&hmdma_mdma_channel0_sw_0, (uint32_t)&SRC_Buf0, (uint32_t)&DST_Buf0, XFR_BUF_SIZE, 1) != HAL_OK)
{
__NOP();
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = 64;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 34;
RCC_OscInitStruct.PLL.PLLP = 1;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 3072;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
/**
* Enable MDMA controller clock
* Configure MDMA for global transfers
* hmdma_mdma_channel0_sw_0
* node_mdma_channel0_sw_1
*/
static void MX_MDMA_Init(void)
{
/* MDMA controller clock enable */
__HAL_RCC_MDMA_CLK_ENABLE();
/* Local variables */
MDMA_LinkNodeConfTypeDef nodeConfig;
/* Configure MDMA channel MDMA_Channel0 */
/* Configure MDMA request hmdma_mdma_channel0_sw_0 on MDMA_Channel0 */
hmdma_mdma_channel0_sw_0.Instance = MDMA_Channel0;
hmdma_mdma_channel0_sw_0.Init.Request = MDMA_REQUEST_SW;
hmdma_mdma_channel0_sw_0.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER;
hmdma_mdma_channel0_sw_0.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
hmdma_mdma_channel0_sw_0.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
hmdma_mdma_channel0_sw_0.Init.SourceInc = MDMA_SRC_INC_BYTE;
hmdma_mdma_channel0_sw_0.Init.DestinationInc = MDMA_DEST_INC_BYTE;
hmdma_mdma_channel0_sw_0.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
hmdma_mdma_channel0_sw_0.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
hmdma_mdma_channel0_sw_0.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
hmdma_mdma_channel0_sw_0.Init.BufferTransferLength = 1;
hmdma_mdma_channel0_sw_0.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
hmdma_mdma_channel0_sw_0.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
hmdma_mdma_channel0_sw_0.Init.SourceBlockAddressOffset = 0;
hmdma_mdma_channel0_sw_0.Init.DestBlockAddressOffset = 0;
if (HAL_MDMA_Init(&hmdma_mdma_channel0_sw_0) != HAL_OK)
{
Error_Handler();
}
/* Initialize MDMA link node according to specified parameters */
nodeConfig.Init.Request = MDMA_REQUEST_SW;
nodeConfig.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER;
nodeConfig.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
nodeConfig.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
nodeConfig.Init.SourceInc = MDMA_SRC_INC_BYTE;
nodeConfig.Init.DestinationInc = MDMA_DEST_INC_BYTE;
nodeConfig.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
nodeConfig.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
nodeConfig.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
nodeConfig.Init.BufferTransferLength = 1;
nodeConfig.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
nodeConfig.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
nodeConfig.Init.SourceBlockAddressOffset = 0;
nodeConfig.Init.DestBlockAddressOffset = 0;
nodeConfig.PostRequestMaskAddress = 0;
nodeConfig.PostRequestMaskData = 0;
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[SRC_BUF_HALF_SIZE]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf1; //Edited
nodeConfig.BlockDataLength = XFR_BUF_SIZE; //Edited
nodeConfig.BlockCount = 1;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_1, &nodeConfig) != HAL_OK){Error_Handler();}
/* USER CODE BEGIN mdma_channel0_sw_1 */
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_1, 0) != HAL_OK){Error_Handler();}
/* Initialize MDMA link node according to specified parameters */
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[0]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf2;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_2, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_2, 0) != HAL_OK){Error_Handler();}
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[SRC_BUF_HALF_SIZE]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf3;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_3, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_3, 0) != HAL_OK){Error_Handler();}
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[0]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf4;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_4, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_4, 0) != HAL_OK){Error_Handler();}
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[SRC_BUF_HALF_SIZE]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf5;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_5, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_5, 0) != HAL_OK){Error_Handler();}
HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_CPLT_CB_ID, MDMA_TransferCompleteCallback);
HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_ERROR_CB_ID, MDMA_TransferErrorCallback);
HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_BLOCKCPLT_CB_ID, MDMA_TransferBlockCompleteCallback);
/* USER CODE END mdma_channel0_sw_1 */
/* Connect a node to the linked list */
/* Make the linked list circular by connecting the last node to the first */
if (HAL_MDMA_LinkedList_EnableCircularMode(&hmdma_mdma_channel0_sw_0) != HAL_OK)
{
Error_Handler();
}
/* MDMA interrupt initialization */
/* MDMA_IRQn interrupt configuration */
HAL_NVIC_SetPriority(MDMA_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(MDMA_IRQn);
}
/* USER CODE BEGIN 4 */
static void MDMA_TransferCompleteCallback(MDMA_HandleTypeDef *hmdma)
{
__NOP();
}
static void MDMA_TransferErrorCallback(MDMA_HandleTypeDef *hmdma)
{
__NOP();
}
static void MDMA_TransferBlockCompleteCallback(MDMA_HandleTypeDef *hmdma)
{
__NOP();
HAL_MDMA_GenerateSWRequest(&hmdma_mdma_channel0_sw_0);
}
//static void MDMA_TransferBufferCompleteCallback(MDMA_HandleTypeDef *hmdma)
//{
// __NOP();
//}
/* USER CODE END 4 */
/* MPU Configuration */
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x0;
MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
MPU_InitStruct.SubRegionDisable = 0x87;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2023-11-09 4:54 AM
After a week of headscratching I have made it work! For those who struggle with MDMA here is a code using a circular buffered linked list. The SRC_Buffer can simulate an ADC who have filled one half of a buffer using DMA. Then the DMA callback funcitons can trigger the MDMA to transfer the data to bigger buffers fast.
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define SRC_BUF_SIZE 50000 //65472
#define SRC_BUF_HALF_SIZE 25000 //32736
#define DST_BUF_SIZE 25000 //32736
#define XFR_BUF_SIZE 25000 //32736
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
MDMA_HandleTypeDef hmdma_mdma_channel0_sw_0;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_1;
/* USER CODE BEGIN PV */
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_2;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_3;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_4;
MDMA_LinkNodeTypeDef node_mdma_channel0_sw_5;
uint8_t SRC_Buf0[SRC_BUF_SIZE];
uint8_t* SRC_Buf1 = &SRC_Buf0[SRC_BUF_HALF_SIZE];
uint8_t DST_Buf0[DST_BUF_SIZE];
uint8_t DST_Buf1[DST_BUF_SIZE];
uint8_t DST_Buf2[DST_BUF_SIZE];
uint8_t DST_Buf3[DST_BUF_SIZE];
uint8_t DST_Buf4[DST_BUF_SIZE];
uint8_t DST_Buf5[DST_BUF_SIZE];
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Initialize(void);
static void MPU_Config(void);
static void MX_MDMA_Init(void);
/* USER CODE BEGIN PFP */
static void MDMA_TransferCompleteCallback(MDMA_HandleTypeDef *hmdma);
static void MDMA_TransferErrorCallback(MDMA_HandleTypeDef *hmdma);
static void MDMA_TransferBlockCompleteCallback(MDMA_HandleTypeDef *hmdma);
//static void MDMA_TransferBufferCompleteCallback(MDMA_HandleTypeDef *hmdma);
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
unsigned int j = 0;
for(unsigned int i = 0; i < SRC_BUF_SIZE; i++){
SRC_Buf0[i] = j;
j++;
if(j >= 256){
j = 0;
}
}
for(unsigned int i = 0; i < DST_BUF_SIZE; i++){
DST_Buf0[i] = 0;
DST_Buf1[i] = 0;
DST_Buf2[i] = 0;
DST_Buf3[i] = 0;
DST_Buf4[i] = 0;
DST_Buf5[i] = 0;
}
__NOP();
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_MDMA_Init();
/* USER CODE BEGIN 2 */
if (HAL_MDMA_Start_IT(&hmdma_mdma_channel0_sw_0, (uint32_t)&SRC_Buf0, (uint32_t)&DST_Buf0, XFR_BUF_SIZE, 1) != HAL_OK)
{
__NOP();
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = 64;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 34;
RCC_OscInitStruct.PLL.PLLP = 1;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 3072;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
/**
* Enable MDMA controller clock
* Configure MDMA for global transfers
* hmdma_mdma_channel0_sw_0
* node_mdma_channel0_sw_1
*/
static void MX_MDMA_Init(void)
{
/* MDMA controller clock enable */
__HAL_RCC_MDMA_CLK_ENABLE();
/* Local variables */
MDMA_LinkNodeConfTypeDef nodeConfig;
/* Configure MDMA channel MDMA_Channel0 */
/* Configure MDMA request hmdma_mdma_channel0_sw_0 on MDMA_Channel0 */
hmdma_mdma_channel0_sw_0.Instance = MDMA_Channel0;
hmdma_mdma_channel0_sw_0.Init.Request = MDMA_REQUEST_SW;
hmdma_mdma_channel0_sw_0.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER;
hmdma_mdma_channel0_sw_0.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
hmdma_mdma_channel0_sw_0.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
hmdma_mdma_channel0_sw_0.Init.SourceInc = MDMA_SRC_INC_BYTE;
hmdma_mdma_channel0_sw_0.Init.DestinationInc = MDMA_DEST_INC_BYTE;
hmdma_mdma_channel0_sw_0.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
hmdma_mdma_channel0_sw_0.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
hmdma_mdma_channel0_sw_0.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
hmdma_mdma_channel0_sw_0.Init.BufferTransferLength = 1;
hmdma_mdma_channel0_sw_0.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
hmdma_mdma_channel0_sw_0.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
hmdma_mdma_channel0_sw_0.Init.SourceBlockAddressOffset = 0;
hmdma_mdma_channel0_sw_0.Init.DestBlockAddressOffset = 0;
if (HAL_MDMA_Init(&hmdma_mdma_channel0_sw_0) != HAL_OK)
{
Error_Handler();
}
/* Initialize MDMA link node according to specified parameters */
nodeConfig.Init.Request = MDMA_REQUEST_SW;
nodeConfig.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER;
nodeConfig.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
nodeConfig.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
nodeConfig.Init.SourceInc = MDMA_SRC_INC_BYTE;
nodeConfig.Init.DestinationInc = MDMA_DEST_INC_BYTE;
nodeConfig.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
nodeConfig.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
nodeConfig.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
nodeConfig.Init.BufferTransferLength = 1;
nodeConfig.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
nodeConfig.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
nodeConfig.Init.SourceBlockAddressOffset = 0;
nodeConfig.Init.DestBlockAddressOffset = 0;
nodeConfig.PostRequestMaskAddress = 0;
nodeConfig.PostRequestMaskData = 0;
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[SRC_BUF_HALF_SIZE]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf1; //Edited
nodeConfig.BlockDataLength = XFR_BUF_SIZE; //Edited
nodeConfig.BlockCount = 1;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_1, &nodeConfig) != HAL_OK){Error_Handler();}
/* USER CODE BEGIN mdma_channel0_sw_1 */
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_1, 0) != HAL_OK){Error_Handler();}
/* Initialize MDMA link node according to specified parameters */
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[0]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf2;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_2, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_2, 0) != HAL_OK){Error_Handler();}
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[SRC_BUF_HALF_SIZE]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf3;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_3, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_3, 0) != HAL_OK){Error_Handler();}
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[0]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf4;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_4, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_4, 0) != HAL_OK){Error_Handler();}
nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[SRC_BUF_HALF_SIZE]; //Edited
nodeConfig.DstAddress = (uint32_t)DST_Buf5;
if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_5, &nodeConfig) != HAL_OK){Error_Handler();}
if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_5, 0) != HAL_OK){Error_Handler();}
HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_CPLT_CB_ID, MDMA_TransferCompleteCallback);
HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_ERROR_CB_ID, MDMA_TransferErrorCallback);
HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_BLOCKCPLT_CB_ID, MDMA_TransferBlockCompleteCallback);
/* USER CODE END mdma_channel0_sw_1 */
/* Connect a node to the linked list */
/* Make the linked list circular by connecting the last node to the first */
if (HAL_MDMA_LinkedList_EnableCircularMode(&hmdma_mdma_channel0_sw_0) != HAL_OK)
{
Error_Handler();
}
/* MDMA interrupt initialization */
/* MDMA_IRQn interrupt configuration */
HAL_NVIC_SetPriority(MDMA_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(MDMA_IRQn);
}
/* USER CODE BEGIN 4 */
static void MDMA_TransferCompleteCallback(MDMA_HandleTypeDef *hmdma)
{
__NOP();
}
static void MDMA_TransferErrorCallback(MDMA_HandleTypeDef *hmdma)
{
__NOP();
}
static void MDMA_TransferBlockCompleteCallback(MDMA_HandleTypeDef *hmdma)
{
__NOP();
HAL_MDMA_GenerateSWRequest(&hmdma_mdma_channel0_sw_0);
}
//static void MDMA_TransferBufferCompleteCallback(MDMA_HandleTypeDef *hmdma)
//{
// __NOP();
//}
/* USER CODE END 4 */
/* MPU Configuration */
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x0;
MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
MPU_InitStruct.SubRegionDisable = 0x87;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.