2018-03-30 5:48 AM
I'm testing one application with 3 differente device that send a message with random command ID and random data on CAN bus every random timeout: two devices with two STM32L433 nucleo and one with STM32F446 nucleo and with TJA1044T NXP transceivers.
I implemented firmware starting with STMCube (rev. 4.0) and added my application code with all corrections that I found in the community.For first test the command ID random range was between 0 to 50 and the timeout random range was from 10ms to 1s. In this case all work enough fine without errors or packet lost.
In second test I reduced the timeout random range and was between 1ms to 10ms. In this case some errors appear and some packet lost; In particular the most freqeuntly errors was BIT ERROR (BR error).
To stress the application again I reduced the command ID random range to 1 (only command ID 0) and set the timeout to 1ms fixed: every ms all the boards (not sincronized) send the same command ID. In this case the number of errors (BOF, STF, FOR, ACK BR and BD) and lost packets increase a lot.
To evaluate the number of errors and lost packets, I implemented specific counters
that I can read by PC SerialPort when the test is stoped.The frequency of CAN bus is 1Mbit/s, I calculated the timing by
/external-link.jspa?url=http%3A%2F%2Fwww.bittiming.can-wiki.info%2F
(Tq = 5ns, BS1 = 13, BS2 = 2, SJW = 1) and I used a very short cable (about 30cm).
In alltests the number of sent packet by every board are about 000.
My question is: is normal this behavior? I didn't found materials in intertet about this. #can #stm32f4 #stm32l4 Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-04-03 7:36 AM
I'd guess 'Error Passive', i.e. error count reaches 256.
2018-04-03 7:41 AM
In our network(s), each node includes his node ID in it's messages, which is unique (like a IP address in TCP/IP networks).
Ok, we was thinking the same idea.
Thanks.2018-04-03 7:45 AM
Ok it could be but the device enter in 'Error Passive' only if counter TEC or REC are greater than 127 and this counters do not increase if arbitration lost.
2018-04-06 10:36 AM
I have tried the system with 3 different commands ID (0, 1 and 2) and every device send only one command ID: in this way all the system works correctly and no error or packets lost are generated.
Thank you very much!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.