2025-03-06 11:37 PM - edited 2025-03-06 11:39 PM
Hi
Community,
I am working with an STM32H723 microcontroller and have configured the OctoSPI interface as follows:
In my setup, HyperRAM and HyperFlash share the same data lines in multiplexed mode. HyperRAM is connected to OctoSPI1, and HyperFlash is connected to OctoSPI2.
OctoSPI2 Initialization Code
OSPIM_CfgTypeDef sOspiManagerCfg = {0};
OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};
hospi2.Instance = OCTOSPI2;
hospi2.Init.FifoThreshold = 1;
hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;
hospi2.Init.DeviceSize = 24;
hospi2.Init.ChipSelectHighTime = 2;
hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi2.Init.ClockPrescaler = 2;
hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
hospi2.Init.ChipSelectBoundary = 0;
hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;
hospi2.Init.MaxTran = 128;
hospi2.Init.Refresh = 0;
if (HAL_OSPI_Init(&hospi2) != HAL_OK)
{
Error_Handler();
}
sOspiManagerCfg.ClkPort = 1;
sOspiManagerCfg.DQSPort = 1;
sOspiManagerCfg.NCSPort = 2;
sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_1_HIGH;
sOspiManagerCfg.Req2AckTime = 1;
if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
sHyperBusCfg.RWRecoveryTime = 0;
sHyperBusCfg.AccessTime = 10;
sHyperBusCfg.WriteZeroLatency = HAL_OSPI_NO_LATENCY_ON_WRITE;
sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;
if (HAL_OSPI_HyperbusCfg(&hospi2, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
HyperFlash Read Function:
uint16_t FlashRead(uint32_t word_address, uint8_t *buffer, size_t buffer_size)
{
OSPI_HandleTypeDef *hOSPI = &hospi2;
HAL_StatusTypeDef halErr = HAL_OK;
OSPI_HyperbusCmdTypeDef sCommand = {0};
uint32_t address = word_address << 1; // convert to bytes address
/* Initialize the read command */
sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
sCommand.Address = address;
sCommand.DQSMode = HAL_OSPI_DQS_ENABLE;
sCommand.NbData = buffer_size;
/* Configure the command */
halErr = HAL_OSPI_HyperbusCmd(hOSPI, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
if (halErr != HAL_OK)
{
Error_Handler();
}
/* Reception of the data */
halErr = HAL_OSPI_Receive(hOSPI, buffer, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
if (halErr != HAL_OK)
{
Error_Handler();
}
return halErr;
}
I am encountering a verification issue after downloading XIP firmware into HyperFlash.
Specifically, data matches up to address 0x964b0. Beyond this address, discrepancies occur.
For instance, the expected bytes are [FE, 5F, E0, 01, 27, 5D, E0] from address 0x964b0. Reading 2 bytes at a time yields correct data. However, an 8-byte burst read results in [FE, 5F, E0, 03, 27, 5D, E0], indicating a 1-bit error.
Modifying the XIP firmware sometimes resolves or shifts the error to another address. Notably, if an error occurs in a specific XIP firmware version, it consistently fails at the same address. The error address within the same firmware is not random. Read test wan't done in memory map mode.
I have utilized DelayBlock_Configure() with various combinations of PhaseSel and units but have not identified a stable value.
I am seeking suggestions to resolve this bit-flipping error. Has anyone experienced similar issues or can provide insights into potential causes and solutions?
2025-03-07 12:38 AM
Hello @blanc6389,
Which HyperRam and HyperFlash memories are you using? Could you please share the memories datasheets?
I recommend you to check the delay block configuration and the calibration.
For that, I advise you to refer to this example DLYB_OSPI_PSRAM_ExhaustiveTuning and this FAQ How to calibrate the delay block with the OCTOSPI interface and check the delay block calibration.
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-07 1:03 AM
I use the following flash and ram.
HyperRam: Infineon S70KS1282
HyperFlash: Infineon S26KS128
U5 and H7 have different DLYB functions in the LL driver. However, I tried using DelayBlock_Configure() on H7 to set PhaseSel and units as done in DLYB_OSPI_PSRAM_ExhaustiveTuning. None of the combinations worked—it usually fails on the second attempt of the read test at the same address, where the read data does not match.
Additionally, I use DelayBlock_Enable() after initializing OctoSPI, with the OctoSPI clock set to freerunning. However, it always returns a timeout error.
2025-03-07 3:52 AM
Hello @blanc6389,
Is the cache enabled?
I recommend disabling the cache to avoid masking issues.
I advise you to look at this discussions may help you: Help needed for tuning 64Mb HYPERRAM (S27KL0642DPBHI020) on STM32H735IGT6.
Please make sure that you configure the memory and the octo-SPI controller to have at least six clock cycles of latency. Because, when the DQS signal is used for HyperBus™ memories, and the number of latency clock cycles programmed in TACC[7:0] is lower than six, a deadlock occurs during read operations. I recommend you to check the STM32H723 errata sheet and precisely section 2.8 OCTOSPI.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.