2008-04-24 10:50 PM
Build the demonstration project STM3210B-eval
2011-05-17 3:31 AM
Hi everybody,
I have since this morning the STM3210B-EVAL/A. I tried the flash programming by the UART, using the software flash loader demonstrator, i erased the flash memory of the evaluation card, so the demonstration firmware in order to download my own program. Now i want to download the demonstration firmware again. I downloaded from the ST site web the firmware with the RIDE project. I open it with Ride7, but I can't build the firmware i have an error at the end like '' Region Flash overflowed by 6232 bytes'', so i can't download the firmware... :-Y I don't know why and so how to resolve the problem.. Can you help me please ...? Really thank you ! and i promise, when i will be a pro of the STM32 i will help on this forum !!!! ^^ THANK YOU !!! :)2011-05-17 3:31 AM
Hi again !!
It's ok now, i succeded to download the demonstration firmware on the evaluation board but using dFuSe . But i have still problems when i went to build the Ride project of the demonstration ....i think perhaps it is because there is all the program ( for the internal flash and for the external flash ) and so it's why there is written ''Region flash overflow''...maybe i don't know !2011-05-17 3:31 AM
You are right.
You need to set the ''starter kit limitation'' option to ''No'' (see attached image).2011-05-17 3:31 AM
Thnk you very much, it's ok now ! Thanks again :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.