2017-09-21 12:05 PM
I exported my project with the latest STM32CubeMX 4.22.1 for our firmware which is for a board with an STM32F429NGH6 and the resulting code has 2 build errors. Here is the problem code with the error lines in BOLD:
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
PeriphClkInitStruct.PLLI2S.PLLI2SN = 192; PeriphClkInitStruct.PLLI2S.PLLI2SM = 25; PeriphClkInitStruct.PLLI2S.PLLI2SR = 3; PeriphClkInitStruct.I2SClockSelection = I2S_CLOCK_PLL; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }This issue is that for
STM32F429NGH6, the PLLIS2M and I2SClockSelection are not present in the structures.
With prior versions of STM32CubeMX these lines simply were not present in the generated code. I will delete them and see if the project builds/runs correctly. I suspect it will.
Here is what I did to cause this problem (but probably less is required):
Create a project for the STM32F429NGH6 chip.
In the RCC
Set HSE to Crystal/Ceramic Resonator
Set LSE to Crystal/Ceramic Resonator
Thanks,
Craig
#stm32f429-build-error"-"i2s-clock"-stm32cubemx"2017-10-13 12:17 AM
Hello
Broadbooks.Craig
,I thank you first for your feedback.
I confirm that those parameters are not use by your SoC family.
This is a CubeMX code generation issue.
Internal ticket has been raised for correction.
Kind regards
Sirma
2017-10-13 1:21 AM
This will be corrected in Cube version 4.23
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.