2018-08-27 3:47 PM
Hi
I wrote a little CEC application. Unfortunatly communication with other devices didn't work well.
I used a logic analyzer to find the problem.
The error is in the IRQ function HAL_CEC_IRQHandler:
[...]
if((reg & CEC_FLAG_TXBR) != RESET)
{
if (hcec->TxXferCount == 0U)
{
/* if this is the last byte transmission, set TX End of Message (TXEOM) bit */
__HAL_CEC_LAST_BYTE_TX_SET(hcec);
hcec->Instance->TXDR = *hcec->pTxBuffPtr++;
}
else
{
hcec->Instance->TXDR = *hcec->pTxBuffPtr++;
hcec->TxXferCount--;
}
/* clear Tx-Byte request flag */
__HAL_CEC_CLEAR_FLAG(hcec,CEC_FLAG_TXBR);
}
[...]
The error is in line if (hcec->TxXferCount == 0U)
Correct is if (hcec->TxXferCount == 1U)
Else an additional wrong byte is sent. This confuses other members on the bus.
In my case my TV didn'T accept the messages. After the fix everything is fine.
Can anybody confirm this bug?
Is it sufficient to post the bug here or is ther another bug tracker? I havn't found one yet.
Best regards,
Tilo
Solved! Go to Solution.
2018-09-12 7:08 AM
The bug is confirmed and is logged.
The explanation is that when the last byte is going to be transmitted, TxXferCount is still 1, not 0, as it's decremented only after writing TXDR.
But for this reason, the TXBR interrupt will be invoked one additional time (possibly reading past the end of the transmit buffer!) and an unknown value will be appended to the message.
To avoid this, it is better to correct with:
if (--hcec->TxXferCount == 0U) /* pre-decrement the size before the comparison */
Best Regards
Christophe
2018-09-12 7:08 AM
The bug is confirmed and is logged.
The explanation is that when the last byte is going to be transmitted, TxXferCount is still 1, not 0, as it's decremented only after writing TXDR.
But for this reason, the TXBR interrupt will be invoked one additional time (possibly reading past the end of the transmit buffer!) and an unknown value will be appended to the message.
To avoid this, it is better to correct with:
if (--hcec->TxXferCount == 0U) /* pre-decrement the size before the comparison */
Best Regards
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.