2017-01-31 6:33 AM
Hello guys,
I have problem with bootloader on STM32F427xx.
Bootloader: 0x08000000 ---128Kb
APP: 0x08020000 ----512Kb
In Linker Script for App, the ResetHandler located at
.start 0x08020200 :
{ . = ALIGN(4); KEEP(*(.start)) /* Startup code */ . = ALIGN(4); } > FLASHbut when I tried to executed these:
#define APPLICATION_ADDRESS (0x08020000UL)
pFunction Jump_To_Application;
uint32_t JumpAddress;SCB->VTOR = FLASH_BASE | 0x20000;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4 + 0x200); Jump_To_Application = (pFunction) JumpAddress;Jump_To_Application();
I couldn't jump into App section.
Can you help me pls, thanks!
PS: I use Jlink Debugger.
2017-01-31 3:57 PM
I tested it with the code above and it works fine.
#define APPLICATION_ADDRESS (uint32_t)
0x08020000
//
Bootloader
Test code{
printf('\n\n JUMP USER FW -->\n'); /* Test if user code is programmed starting from address 'APPLICATION_ADDRESS' */ if (((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0x2FFE0000 ) == 0x20000000) { /* Jump to user application */ JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4); JumpToApplication = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS); JumpToApplication(); } }// Application
Test code
-> system_stm32f4xx.c SystemInit() function (
Application project )
VECT_TAB_OFFSET : The value needs to be modified in application project.
#define VECT_TAB_OFFSET
0x20000
Please test it.
2017-01-31 4:21 PM
Why on earth do you have the +0x200 in there?
JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4 + 0x200);
You are loading an ADDRESS from the vector table, the ADDRESS should point to the ResetHandler
Also, this would be less ambiguous
SCB->VTOR = APPLICATION_ADDRESS;
If you are unsure about addresses you can print them out, or step the code with a debugger. You can look at the .MAP file of the APP to understand if you are going to the right functions
2017-02-02 7:44 AM
I have a configuration similar to you with a custom flashloader located at 0x0802 0000 and my application at 0x0804 0000. The way I found easier for us is to reconfigure the option bytes and reset the CPU.
here is my function to do it
void StartIPLB2FlashLoaderCode(void)
{
HAL_StatusTypeDef Status = HAL_ERROR;
//Address = (<ADDR_BOOT_PIN_1> << 16) | <ADDR_BOOT_PIN_0>
uint32_t Address = 0x00400088;
//Clear Any Pending Flash Flags
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR |\
FLASH_FLAG_PGAERR | FLASH_FLAG_PGPERR| FLASH_FLAG_ERSERR);
if(HAL_FLASH_Unlock() == HAL_OK)
{
//Set Half-Word write operation
FLASH->CR &= CR_PSIZE_MASK;
FLASH->CR |= FLASH_PSIZE_HALF_WORD;
HAL_FLASH_Lock();
if(HAL_FLASH_OB_Unlock() == HAL_OK)
{
if(FLASH_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE) == HAL_OK)
{
FLASH->OPTCR1 = Address;
Status = HAL_FLASH_OB_Launch();
}
HAL_FLASH_Lock();
}
}
if(Status == HAL_OK)
{
HAL_NVIC_SystemReset();
}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.