2024-04-23 1:07 PM
I am using an STM32 G474RE NUCLEO board. Is it necessary for me to configure the BOOT0 pin and the BOOT bits in the FLASH_OPTR register if I am going to program the chip using the SWDIO and SWCLK pins with an ST-LINK V2?
Solved! Go to Solution.
2024-04-23 1:14 PM - edited 2024-04-23 1:14 PM
Hello,
No need to touch anyhting if you plan to use the debug.
Keep boot0 pin tied to GND and Boot bits to default state.
2024-04-23 1:14 PM - edited 2024-04-23 1:14 PM
Hello,
No need to touch anyhting if you plan to use the debug.
Keep boot0 pin tied to GND and Boot bits to default state.
2024-06-28 11:34 AM
Hello,
Reading this thread I need a bit of clarity.
I currently use mostly STM32L series controllers. On board builds I use PA13,PA14 to a simple 5 pin header along with VDD, GND and nRST. I use the ST-LINK pod to flash and debug. I'm using IAR EWARM to program and debug, this has been working fine for years.
I want to move to the STM32G series. If I plan to use the G0 devices in the same manner as with the L4, do I need to add a (0 ohm) pull down to GND on SWCLK (PA14-BOOT0)? If doing this will this allow it to boot normally with the ST-LINK attached?I'm under the impression that it will but don't want to commit to a build unless I do. The post above from SofLit says: "Keep boot0 pin tied to GND and Boot bits to default state." I assume the NUCLEO board has a shunt/pull down attached to PA14...
I think I understand that I can then change the bits at some point to change the flash mode if required.
Thanks!
Gary
2024-07-01 1:21 AM
Hello @roger99 ,
I suggest you to open a new thread for your questions.
Thank you for your understanding.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.