cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG - simultaneously Master&Slave

ann
Associate II

i want to use a board as master and slave simultaneously.  role= GAP_PERIPHERAL_ROLE | GAP_CENTRAL_ROLE; 

now, i am able to establish a connection between a Master&Slave board and a slave board. however, when i want to set the Master&Slave board into discoverable mode after that,

 an error occurs: error code is 0x0C BLE_ERROR_COMMAND_DISALLOWED .

Why is that? and how to solve this problem?

if i set the device into discoverable mode directly (do not connect it with slave A), the command was successfully.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
embedded_guy
Associate

Hi,

Not sure if you resolved this, but I'm seeing something similar...I think.

I am setting up my advertising packet with extended (custom) information. I have seen that if I use more than one advertising data handle when calling aci_gap_set_advertising_enable, I get that error as well (0x0C DISALLOWED). If I only send in one handle, then the enable command doesn't return an error.

However, I have also seen that the slave module will still connect, even with this error returned.

Let me know if you were able to figure this out.

Thanks,

Anthony

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.