2018-05-08 8:13 AM
Hi,
i'm working with stm32f415RG and i have a strange behaviuor with RTC.
I configured RTC with LSE
Alarm A Internal Alarm
Alarm B Internal Alarm
WakeUp : internal wakeup
Tamper1 Routed to AF1
TimeStamp on Tamper detection event is not saved
After init of RTC, BKP0R register is setted with 0x32F2 value, but immediatly after a tamper event, this value return to 0x00000.
Its normal ?
Sorry for my english
2018-05-08 8:25 AM
Solved,i found the answer:
RTC_BKPxR, where x=0 to n backup registers (80 bytes), are reset when a tamper
detection event occurs. These registers are powered-on by VBAT when VDD is switched off,so that they are not reset by a system reset, and their contents remain valid when the deviceoperates in low-power mode.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.