2009-02-13 8:07 PM
Bit banding SRAM when booting from SRAM?
2011-05-17 4:02 AM
Does the bit band alias base address for the SRAM (0x22000000) change to 0x02000000 if I select to boot from system memory block (SRAM)?
I have read that the SRAM will appear at 0x00000000 if embedded SRAM is selected as boot space.2011-05-17 4:02 AM
No, it doesn't. The bit-band is fixed at 0x22000000 and 0x42000000. If the memory is remapped to 0x0 by the memory system, the processor will not carry out bit-band operation to it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.