2017-02-18 4:32 PM
Sorry if that's known but I've only learned today that on eBay you can get a board which tries to look like stm32f4discovery while it's only a copy
on eBay they list it as 'Stm32f4 Discovery Stm32f407' (spelled with a space)
note how audio connector is green
note lack of ST logonote how all LEDs are blueand serial-over-USB does not work on this example
and it costs above $19.90 the real one costs in the USA!
2017-02-18 6:18 PM
The original STM32F4-DISCO didn't support the USB/VCP connection, even the newer STM32F4-DISC1 board you'd have to solder wires to the ST-LINK's STM32F103 part.
Both buttons look to be black also, and the ground jumpers at the top don't appear to be populated.
Lot of fake stuff on eBay. A clear photo might work better than the video here.
2017-02-18 6:42 PM
serial-over-USB - I mean on the micorUSB of the stm32f407 chip with my custom firmware. will ask that guy for a picture - the board is in Norway I am not
2017-02-18 11:42 PM
This board may be Chinese FAKE.
There is a lot of copy/fake/clone boads(even mcu) on ebay and aliexpress.
2017-02-19 5:22 AM
Note LD0 / LD1 modification
http://i.imgur.com/vyVNkje.jpg
scary soldering
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.