STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lost access to STM32G030 micro

In a recent design I needed an additional pin and I configured the PA13 / SWDIO pin as a GPIO input.All going fine, code works, but then this happened: After I program the chip in automatic mode and set the option byte rdp to 0xBB I can't connect aga...

KPN1 by Associate III
  • 676 Views
  • 4 replies
  • 0 kudos

SRAM3 memory block availability for STM32H742xI/G

Hi,In STM32H742xI/G datasheet (DS12110 Rev 8), the SRAM3 memory block is not specified in the "Table 7. Flash memory and SRAM memory mapping" but I can see the availability of the SRAM3 in the generated .map file.Can someone please confirm, it is typ...

palanib_0-1765419963955.png palanib_1-1765420104807.png
palanib by Associate
  • 491 Views
  • 1 replies
  • 0 kudos

STM32U073CCT6 - STOP MODE 2 Power Consumption

Hi We are using an STM32U073CCT6 on a battery-powered board. We need to put the processor in low-power mode to increase battery life. The current in STOP MODE 2 is about 20uA. To address some issue related to the power supply and our hardware, we put...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.