STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Propogation delay from comarator to timer to start ADC sampling

I have a project to use the STM32L496 to sample an analog pulse for processing.The sceraio as followes:Input guassain pulse will be fed to postive comparator input, the negative terminal will be set by the DAC. Once the signal above the DAC threshold...

ahaj by Associate
  • 1039 Views
  • 0 replies
  • 0 kudos

Resolved! ADC Value Distortion

Hello,I have been experiencing a problem with the usage of the internal ADC on my STM32L476RG Nucleo64 development board. Unfortunately I have not been able to find similar problems online or in the forums.I would like to use the highest possible sam...

pythomancer_0-1707984906191.png pythomancer_1-1707984934444.png pythomancer_2-1707984962233.png pythomancer_3-1707985262505.png

USB OTG Sample

Hi team,            I am working on USB recently, wanted to try the OTG application. I want to understand the OTG working is there any project or sample code or docs available for the same? if yes, plz share me the reference. Thanks,Shikamru

Shikamaru by Associate III
  • 5346 Views
  • 4 replies
  • 0 kudos

STM32L031F6 ADC read multiple channels

Hi,can anyone please provide help/sample/tutorial on how to read two different ADC Pins on my STM32L031F6 using STM32CubeIDE, idealy without DMA, but with would also work.I have two analog signals on PA2 and PA3 and would like to read them. I suppose...

durpex by Associate
  • 8166 Views
  • 4 replies
  • 0 kudos

IrDA is not working at low system clock

Hello All, I am working on a custom desing board having STM32L053C8T6. It uses IrDA setup for the communication. I have setup the MCU at 131KHz as System clock to achieve Low power consumption (currently 65uA). Now i need to communicate with the PC u...

clockstm32.PNG
Sakaz by Associate
  • 1981 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U5xx: SPI3 slave fails at 80 MHz

I use OCTOSPI as SPI master and listen via SPI3 as Slave (in SW NCS mode) what was sent from master.SPI3 Slave fails for clock speed 80 MHz (larger as 54 MHz:(Symptoms:the data bytes on SPI3 slave are wrong (they look like shifted by one bit)running ...

tjaekel by Lead
  • 2450 Views
  • 3 replies
  • 1 kudos

VBAT and Power Controll

Hi.I made a custom board using stm32f767connect Coincell (CR1220) to VBAT and turn it off, I think I'm going into some modeSometimes it does not go into the main when the power is turned on again, and the battery life is short when the power is turne...

Octo83 by Associate
  • 1528 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.