STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot Write register

Hello guys! I have a problem. I need to use HAL_RTCEx_SetSynchroShift function from HAL to modify the subseconds of the RTC module. The problem is that this function cannot work because the REFCKON bit from Control Register is set(1). First, I do not...

Phvne by Associate II
  • 579 Views
  • 0 replies
  • 0 kudos

fx_media_open timing is too slow. How do I speed this up?

Folks, I have a device that installs into another product and provides SRAM for code execution for the other device.  The device my board plugs into has a fixed 500ms RESET generator that hold off the host device CPU for that much time.  During this ...

VT_Jim_0-1717075480190.png
VT_Jim by Associate III
  • 2513 Views
  • 3 replies
  • 0 kudos

STM32h7 problem with SDMMC Initialization

Hello,I'm using an STM32h753i-eval2 board and trying to access an SD card through the SDMMC peripheral.I have my RCC set on Master Clock Output 1.I has the SDMMC external transceiver present set to no.System clock mux is set to HSIPLL Source is HSIUs...

TLuke.2 by Associate II
  • 8089 Views
  • 8 replies
  • 0 kudos

STM32F0 TIM2 vedio tutorials

Posted on November 18, 2014 at 16:14Dear All,It would be much appreciated, if some one can give me a video links that explaining each every step of operation of STM 32F0 TIM2 or any timer Thanks in advance

pic_micro by Associate II
  • 1797 Views
  • 5 replies
  • 0 kudos

ADC always returns 0

I'm trying to read 2 ADC channels (ch 0-1) on an STM32G030C8T6 but the only result I can get from the ADC is a 0.I've confirmed the voltages I'm trying to read are at ~1.6V and that the VREF+ pin is at ~2.7V using a multimeter so I dont believe its a...

0693W00000YAqalQAD.png
MMurr.2 by Associate II
  • 8444 Views
  • 7 replies
  • 1 kudos

STM32H7x SPI Slave FIFO data loading

Hello,We have been trying to use the STM32H747I-DISCO to act as a SPI slave which should respond to a command byte, behaving similarly to how a sensor or EEPROM might.That is, the fist byte sent from the master will be a command and our slave device ...

2024-06-21-17-11-06-image.png 2024-06-24-08-29-28-image.png 2024-06-24-08-46-26-image.png
vegac by Associate II
  • 2821 Views
  • 3 replies
  • 0 kudos

Resolved! FDCAN filtering issue on G473

Hello, I am writing FDCAN driver filtering function for the open source ChibiOS RTOS, both for FdCanV2(H7) and FdCanV1(G4) For the H7 side, all went easy, and the driver works as intended. On the G4 side,  FdCanV1 is a bit simpler (the ram buffer is ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.