STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F411: how to handle I2C Errors

I am using the I2C code in STM32Cube_FW_F4_V1.26.0\Projects\STM32F411E-Discovery\Examples\I2C\I2C_TwoBoards_ComPolling as base to write my own I2C firmware.I would say the HAL library in stm32f4xx_hal_i2c.c is quite useful and covers all I2C communic...

HDaji.1 by Senior
  • 19055 Views
  • 12 replies
  • 1 kudos

Resolved! STM32F103C8T6 UART 8-bits and Even parity

Hii I am using STM32F103C8T6 controller. In this controller I am using the UART1 and UART2 transmitting and receiving data. In UART1 I adjust 9600 Baud rate, 8-data bits, None parity and 1 stop in these configuration I am transmitting and receiving d...

Yeswanth by Associate II
  • 2704 Views
  • 4 replies
  • 2 kudos

ADC channel numbers incorrect on datasheet STM32U031R8T6

Hi, I am just trying to run adc in discontonous mode to measure some voltate from two resistor divider connected on channel 6 (PA1) and channel 7 (PA2) and also Vref from internal channel 12 as per datasheet. see below screenshot from DS14581- Rev2 ...

KSB_0-1721264870489.png KSB_2-1721265399785.png
KSB by Associate II
  • 1593 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G030K6 usart bootloader

 Hi, I have a custom board with STM32G030K6 and I wish to use the buildin usart bootlaoder. I have checked the AN3155 and AN2606, but I still cant figure out how to enter into the bootloader. I found that for my MCU, I need Pattern 11 to activate boo...

KlemenDS_0-1724915993477.png
KlemenDS by Associate II
  • 2455 Views
  • 4 replies
  • 1 kudos

SPI txCRC wrong value

Hello,I am using SPI with crc enabled on stm32f429ig.The problem is: if master's SCK's gpio speed is configured as medium, everything works fine. BUT if it is set to veryhigh, transmitted crc (read from TXCRCR register) always calculates a wrong valu...

Dav1d by Associate
  • 1334 Views
  • 2 replies
  • 0 kudos

Resolved! How to handle Variable length receive data via UART?

uint8_t rx_buffer[32], rx_flag, rx_index, rx_data, RxData[32];   void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { if (huart->Instance==USART1) { //if the data is not being received, clear the buffer if(rx_index ==0) { for (int i=0...

TMuka.1 by Associate II
  • 18941 Views
  • 15 replies
  • 3 kudos

STM32H745 FMC PSRAM 16-bit always sends 64-bit

Hello,I am trying to get the FMC to work in 16-bit synchronous mode but I only get an output with 4 clocks (64-bit) instead.In other threads [1], [2] I found that I should either switch the address from 0x60000000 to 0xC0000000 or enable the MPU, but...

fmc.PNG mpu.PNG Kurngop32_0-1701939633228.png
Kurngop32 by Associate III
  • 5659 Views
  • 8 replies
  • 0 kudos

CAN NETWORK

I would like to test an application with the can network, I found some applications on the internet using a blackpill or bluepill like in this website: https://www.micropeta.com/video115, but here I have an STM32F723IEK6 NUCLEO-G474RE and I tested th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.