STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stack problem and privilege mode

Posted on June 16, 2011 at 14:48hi. i am using the STM32f103 chip and i am having all sord of problem that takes me to the Hard Fault inturpt . when i check the SCB->CFSR register i am getting all sord of errors like : ''the processor has attempted ...

ezrab by Associate II
  • 6512 Views
  • 23 replies
  • 0 kudos

USBTMC

Posted on July 04, 2011 at 14:17I want to implement USBTMC with STM32 USB-FS-Device lib and don't know where to start :( Any hints ?

TIM2 in STM32F100C8

Posted on June 30, 2011 at 10:25I m trying to use TIM2 as a general purpose timer to generate an interrupt at every 10mS. void Timer2_Init(void) {     TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;         TIM_TimeBaseStructure.TIM_Period = 10;    ...

ezyreach by Associate II
  • 4589 Views
  • 10 replies
  • 0 kudos

Core cm3

Posted on June 21, 2011 at 10:18extern uint32_t __get_PSP(void); Hello, When I compile an example, I have all these errors, they said incomptabile declaration for all the folowing list: extern void __set_PSP(uint32_t topOfProcStack); extern uint32_t...

cyril2399 by Associate II
  • 1381 Views
  • 2 replies
  • 0 kudos

STM32F100R4H6 SMBus interrupt problem

Posted on July 01, 2011 at 15:21HI..in attach file there's my code. i've to manage smbus using interrupt (no polling allowed). I don't understand why the interrupt doesn't start. The code doesn't me any error. Is it correct manage the smbus protocol...

Calling RTC_Init

Posted on June 27, 2011 at 12:13Good morning everybody! I'm evaluating ST standard device Library with STM32L discovery board. I want to test RTC and so in my main I want to call RTC_Init and so on. So I prepare a RTC_InitType  structure, I create a...

Interupt priorities

Posted on June 28, 2011 at 09:38Hi All, Can anyone explain the difference between the prem and sub interupt priorities.  For example what TIMER_1_IRQ_PREM_PRI and TIMER_1_IRQ_SUB_PRI. -- Thanks #stm32-c-embedded

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.