STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Mass storage - using ST Mass_Storage example code

Posted on August 15, 2011 at 13:32Hi, I'm trying to implement USB mass storage and mass storage bootloader on STM32F103RBT but ... I have a problem with the adapted the code from STM32_USB-FS-Device_Lib_V3.3.0 Mass_Storage example. The ISTR_RESET in...

SPI NSS configuration and use - Help please

Posted on August 01, 2011 at 10:17Please could someone post the details to manage the SPI NSS signal? I want to use the SPI as a full-duplex master (sending and receiving data simultaneously). I have read many posts about the NSS deficiencies in the...

John F. by Senior
  • 6404 Views
  • 6 replies
  • 0 kudos

stm32f207 LCD

Posted on August 08, 2011 at 10:13hi.  i would like to start anew project with stm32f207 with lcd. i know that the stm32f207 can controll lcd throw FSMC bus my question is whats the maximum size of lcd i can use and how do find whitch LCD monitors i...

ezrab by Associate II
  • 5229 Views
  • 10 replies
  • 0 kudos

using ADC

Posted on August 10, 2011 at 22:29hey everyone,it is first time for me programming any kind of processor and trust me i am trying very hard to figure out..i am using STM32VL discovery board in my project work.i have 3 sensors which will give me ADC ...

STM32F207VGT6 OTG FS doesn't start

Posted on August 12, 2011 at 19:06Hello.I have a problem with starting OTG FS in Device mode. I will try to adapt project example ''STM32_USB-FS-Device_Lib_V3.3.0'' for this STM32F-2 chip, but USB doesn't run. For new chip I'll do next: 1. Prepare s...

denlok by Associate II
  • 1552 Views
  • 4 replies
  • 0 kudos

SDIO STM32F215 need help

Posted on August 12, 2011 at 15:05I have no clock on PC12. But when PC12 is OUT mode it is work.  If I run mySDInit() I will see two jump on pc12 ( out mode test ). No clock. Where is the bug?void mySDInit( void ){   uint32_t regSDIO_CLKCR;  GPIO_In...

v239955 by Associate II
  • 1734 Views
  • 4 replies
  • 0 kudos

Switch from HSE to HSI on failure of the HSE?

Posted on August 15, 2011 at 13:50Hello I would like to switch from the HSE oscilator to the HSI oscilator if there is a failure of the HSE oscilator. How can I do that with preserved SYSCLK (64MHz)? The HSI klock is divided på 2 så the PLL would ...

sima2 by Associate III
  • 952 Views
  • 1 replies
  • 0 kudos

[STM32F2xx] 120MHz + 3 wait state = bugs?

Posted on August 09, 2011 at 08:41Hello, Since the beginning of the project on the STM32F205RG, I had hard faults from time to time. These last days, I wrote a hard fault handler as described in Joseph Yiu's book to see why ... and the result was ve...

root by Associate II
  • 4214 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.