STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F151xx vref questions

Posted on September 21, 2011 at 05:20Hi, Vrefint � Looking for a better description of how this voltage is formed/used.  When using an external Vref+, is Vrefint tied to it or to VDDa? How would we expect the PVD and BOR functions to operate if Vre...

STM32L GPIO

Posted on September 17, 2011 at 14:55Hi.I am a student and i must do a project with the STM32L-Discovery using SPI.I found this code:/**  * @brief  Changes the mapping of the specified pin.  * @param  GPIOx: where x can be (A, B, C, D, E or H) to se...

leone1386 by Associate II
  • 1455 Views
  • 2 replies
  • 0 kudos

unlock internal flash memory (readout protected) of STM32W108

Posted on September 19, 2011 at 18:09Hi, I tried to flash an stm32w108 with JLINK but i get an error: Error: Wrong AHB ID (15:3). Expected 0x04770001 (Mask 0x0FFFFFCF), Found 0x00000000 i want to know how could I solve this problem. Sure my microco...

w23 by Associate II
  • 1153 Views
  • 1 replies
  • 0 kudos

stm32 usb library

Posted on September 19, 2011 at 11:45  function as following,  if xfer_len> hnptxsts.b.nptxfspcavail, then fifo space isn't enough /** * @brief  USB_OTG_HC_StartXfer : Start transfer * @param  pdev : Selected device * @param  hc_num : channel number...

yujiu by Associate
  • 801 Views
  • 0 replies
  • 0 kudos

HELP! SIMPLE APP WONT WORK

Posted on September 16, 2011 at 07:57just tryin to send PE.06 high but its not workin. is it my sourcecode? IT DOES compile without error or warnings.#include ''stm32f10x_lib.h''void Clk_Init (void) {   // 1. Clocking the controller from internal HS...

Getting the source of wakeup from STANDBY

Posted on September 17, 2011 at 12:53Hello,I have an application where I have 2 sources that wake my STM32F from STANDBY: RTC and wakeup pin. Both work well as designed (they wake my MCU from STANDBY) but I cannot get the flag to tell what caused th...

juraj2 by Associate II
  • 4409 Views
  • 5 replies
  • 0 kudos

spi1 and dac1 conflict

Posted on September 18, 2011 at 22:38I have observed a conflict between SPI1 and DAC1 on stm32f103ZG micro. When spi1 is initialized first and then DAC1 the spi1 clock shuts down. It is time sensitive, but I manage to make repeatable on stm3210E-EV...

Problem with GPIO

Posted on July 02, 2011 at 16:15Hello, I try turn on and turn off a led when i press the button user1 but can not to do that, So i don´t understand my mistake. I m using Keil with stm32_init.c, i config GPIOA.PIN1 like floating input... the main co...

ivitro by Associate II
  • 1760 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.