STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Configuration

Posted on November 01, 2011 at 16:38Hello, I was learning reading the SPI documentation and there is something I do not understand. In the file stm32f10x_spi.h it is defined: #define SPI_Direction_2Lines_FullDuplex ((uint16_t)0x0000) #define SPI_Dir...

STM32F103ZE RS485 DMA communication problem

Posted on October 31, 2011 at 18:54HI!I have a problem with the following code .. After a few hours to several days. The maximum was to 14 days Data transmission stops working. Receive and transmit works in one task. (BACNET protocol) For DMA uses i...

arsi by Associate
  • 1715 Views
  • 3 replies
  • 0 kudos

TIMER7 INTERRUPT FLAG NOT CLEARING

Posted on October 30, 2011 at 19:12Hello,I have one problem about clearing timer7 interrupt flag at different timer clock prescaler,void TIM7_IRQHandler(void){   if (ih == 0)   ih=1;   else   ih=0; TIM7->SR  = 0x0;}I m setting APB1 presclaer ...

USB CDC (Virtual COM) and DFU (Device Firmware Upgrade)

Posted on October 07, 2011 at 01:22Hi, i m using stm32 cortext m3. Is it normal to have CDC (virtual com port) combine with FDU to become a composite USB device? Is there any example on this? Thanks.This is so that a PC application can perform not o...

etan by Associate II
  • 5924 Views
  • 7 replies
  • 0 kudos

device option bit IWDG

Posted on October 28, 2011 at 20:42I know how to set the IWDG hardware bit using the ST dongle. The production people are going to kill me if I ask them to use an additional dongle. (they use the Keil dongle) Is there another way to enable the hardw...

emalund by Associate III
  • 621 Views
  • 0 replies
  • 0 kudos

STM32-MP3NL/COD - MP3 decoding

Posted on October 28, 2011 at 16:21Hi Does anybody know the status of the proposed MP3 licence per device?http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATA_BRIEF/DM00024441.pdf Cheers, Martin.

STM32F207 and internal USB phy

Posted on September 06, 2011 at 17:17Hi, I am working on a STM32F207 micro controller on a personal Borad.I use 2 USB - A usb OTG on internal phy of pin PA9, PA10, PA12 andPA13 with a mini AB connector   This is the same use onthe eval board - A usb...

axel by Associate II
  • 2077 Views
  • 4 replies
  • 0 kudos

STM32 I2C slave

Posted on October 27, 2011 at 10:18Hi, I configured STM32 I2C as slave. I have a master which read data of a valid STM32 I2C register address and then data of an STM32 I2C not valid register address, which is the data expected on the SDA line? After...

brazov22 by Associate II
  • 1201 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.