STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UFQFPN32 - Stencil recommendations

Does anyone know where I can find STM's solder paste stencil recommendations for UFQFN devices?We are using STM32F051K6U6 however the datasheet only has recommendations for the BGA package of this device, not the QFN.We are getting shorts underneath ...

AMIGD by Associate
  • 1532 Views
  • 1 replies
  • 0 kudos

Resolved! UDP packets no sent on certain ports

Why are UDP packets on port 53600 sometimes sent and visible in Wireshark, but at other times they are not sent? What factors could influence the intermittent transmission of these packets? 

priyazcs by Associate II
  • 1047 Views
  • 1 replies
  • 0 kudos

Self waking up from Standby Mode

HalloI use STM32F779 and want to enter this device in Standby mode and wake up via Wake up pin (PA0). The problem is that everything only works one time correctly or it complete its loop first time just correctly. After the Reset, Microcontroller goe...

Slh by Senior
  • 3683 Views
  • 5 replies
  • 0 kudos

UART via DMA remains busy

HelloI am currently working on a project needing UART via DMA, however when trying to transmit something via this UART nothing is received on the receiving end and the UART remains in HAL_UART_STATE_BUSY_TX.I am also making use of ARM TrustZone.USART...

Resolved! STM32H563 bootloader SPI configuration

Hi,in AN2606 rev 64, I cannot find the SPI settings for STM32H563 bootloader, i e CPOL, CPHA etc. For the other MCU:s in this document, this information is provided.For example H72xxx comes with CPOL = CPHA = low.Using these settings, and a rather sl...

Dimlite by Associate III
  • 2422 Views
  • 4 replies
  • 0 kudos

Resolved! 4 line Nor flash speed during memory map mode

Hi I use STM32H743XI and W25Q256 for my design.And I notice W25Q256 has two speed 133Mhz(W25Q256JV) and 104Mhz(W25Q256FV), currently I use W25Q256FV, since I only use this flash with memory map mode, is it necessary to replace with W25Q256JV? Will th...

ZhouJianQiang_0-1729136629793.png ZhouJianQiang_1-1729136668450.png

STM32 for high speed ADC > 100 MSPS

Hi,My customer wants to design a high speed ADC aquisition system with minimum 100 MSPS rate and 14-bit resolution.The external ADC devices like AD9258 and AD9268 have this capability, which we are proposing.Would it be possible to use a high speed S...

Resolved! STM32 for live streaming

Hi,we would like to add live video playing/streaming to an STM32-based board we are designing that uses MIPI-DSI to drive a touch display, and we are at the stage of choosing the micro.Ideally it would stream from HDMI signal but we can use another i...

Ricko by Senior III
  • 3510 Views
  • 2 replies
  • 3 kudos

Resolved! H723Z external SD Ram clock no signal IS42S16400J-6TL

I'm working on a custom board with a STM32H723ZG. I'm also using external sd ram part  IS42S16400J-6TL found here (https://www.digikey.com/en/products/detail/issi-integrated-silicon-solution-inc/IS42S16400J-6TL/2708625). I've followed the excellent s...

fihes47572_0-1728664562680.png fihes47572_1-1728664583453.png fihes47572_2-1728664605152.png fihes47572_3-1728664611380.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.