STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

quadrature encoder

Posted on December 18, 2011 at 01:56Hi, I am trying to get the quadrature encoder working.  I found and copied code from these forums for setting it up with a different micro controller but the one on the STM32F4 does not support RCC_APB2Periph_GPIO...

stm32l beginner questions

Posted on December 16, 2011 at 16:33Hello,I've recently bought a stm32l-discovery board and I want to start developing for the onboad processor. I  have some previous experience with 8bit atmel microcontrollers but not with (32bit) ARM processors.I ...

luc2 by Associate
  • 843 Views
  • 2 replies
  • 0 kudos

LSI as RTC clock

Posted on December 15, 2011 at 11:24Hi , Is it possible to run RTC with 40khz LSI when power is off and CPU works on battery only? #rtc #lsi

STM32F105 USB Speed, Fifo size

Posted on December 14, 2011 at 20:52Dear all, I've not found a related topic. Right now I've checked with the demo of mass storage device the possible maximum transfer speed. And it looks like ~500kByte/s, for writing to the device. The define at us...

elgerta by Associate II
  • 1604 Views
  • 2 replies
  • 0 kudos

Yagarto vs Raisonance

Posted on December 16, 2011 at 06:51I'm using a makefile to build my application - I'm not a huge fan of IDE's.By setting my PATH environment variable (in Win32 system) to the Raisonance toolchain everything builds fine and runs fine on my STM32F2.B...

carl2399 by Associate III
  • 5154 Views
  • 11 replies
  • 0 kudos

What is the SPI1 address for the DMA controller?

Posted on December 17, 2011 at 04:36I am attempting to transmit SPI1 data using DMA2. What is the SPI1 PeripheralBaseAddr to be used in the following statement? DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)SPI1_DR_ADDRESS;

CC Timer Interrupt (STM32F102RBT6)

Posted on December 16, 2011 at 19:19Using a general purpose timer (TIM3), with a constant frequency I would like to be able to occasionally generate an interrupt on CC3 using a variable count for CCR3.  I do not want to generate a PWM signal or chan...

jmorton by Associate II
  • 2051 Views
  • 2 replies
  • 0 kudos

STM32w108 delay function with Ember stack

Posted on December 16, 2011 at 15:09hi, i have a problem with delay time function of the STM32W108 and EmberZnet stack. so I want a delay time of more than 10 seconds. I used the HAL library and especially the function: halCommonDelayMilliseconds();...

w23 by Associate II
  • 2023 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.