STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32W DBGMCU_IDCODE

Posted on January 26, 2012 at 01:28The STM32F10x series of MCU's make use of the ARM Private Peripheral Bus address 0xE0042000 to implement a MCU IDCODE with a revision ID and a device ID.  I am using the STM32W, and nowhere in the documentation can...

How to build an example from ST distribution?

Posted on January 14, 2012 at 06:08When I try to build an example from ST distribution: STM32F4-Discovery_FW_V1.1.0\Project\Peripheral_Examples\IO_ToggleI get an error complaining of missing stm32f4_discovery.h.This header file is distributed in a f...

ozvena by Associate II
  • 7736 Views
  • 12 replies
  • 0 kudos

Using a Timer as a Divider

Posted on January 25, 2012 at 10:13Hi Can somebody point me in the right direction. I have a peripheral that uses a strange SPI where the data is triggered on both rising and falling edge of the clock. I have heard the i could use a timer as a divid...

0690X0000060505QAA.png
mb2 by Associate II
  • 2464 Views
  • 5 replies
  • 0 kudos

question about startup vector

Posted on January 25, 2012 at 14:44I am learning how STM32 works. I looked at startup file and starup vector using simulator and example project. And I have question (STM32F105): 1. First dword location of vector is stack pointer and it is initializ...

aalmax by Associate II
  • 1115 Views
  • 2 replies
  • 0 kudos

FTP TCP/IP low cost.

Posted on January 24, 2012 at 12:00Hello I am looking for a TCP / IP stack that integrates affordable DCHPclient, ''FTP client'' and filesystem. Ported to a STM32F4xx. LwIP not implemented. NicheLITE requires additional packages. Price? Open-source...

IHS1 by Associate II
  • 1083 Views
  • 2 replies
  • 0 kudos

TIM5_CH1_ETR

Posted on January 23, 2012 at 11:02I need all four channels on TIM5 for input capture. According to the data sheet, TIM5_CH1 is available on PA0. On PH10, a signal called TIM5_CH1_ETR is available. Can I use this pin as a normal channel 1 input, or ...

torleiv by Associate II
  • 2124 Views
  • 4 replies
  • 0 kudos

stm32f107vc usart

Posted on January 23, 2012 at 17:49Hi,I am trying to get the usart to work on the olimex stm32-p107 board. I setup the GPIO ports and USART, but cannot seem to send, or receive any data. Has anyone has this problem? or any ideas?  Here is my code: R...

Did I brick STM32 Discovery Board ?

Posted on May 01, 2011 at 19:54I am new to ARM. I got the STM32 Discovery board.  (STM32F103RGT6 chip) I made a quick code that uses the serial port.(code I copied from Keil website that uses the serial port, and just modified very slightly so it al...

vito_1978 by Associate II
  • 2968 Views
  • 6 replies
  • 0 kudos

DMA Interrupt handler not working

Posted on January 17, 2012 at 17:30I'm using the standard periphery library for this board. The DMA is working correctly in combination with DAC (memory to peripheral transfer) but I can't get the cpu to execute the interrupt handler for DMA1_Stream...

giu by Associate II
  • 1546 Views
  • 1 replies
  • 0 kudos

STM32F4 Discovery not working without reset

Posted on January 23, 2012 at 18:50I have an STM32F4 Discovery board; recently I just had uploaded some code pertaining to the PWM example where I made PD12-15 some PWM signal so I could see it working with the LEDs on board. The program uploaded an...

vaibhav23 by Associate II
  • 2071 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.