STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sourcery CodeBench Lite for STM32F4xx

Posted on March 09, 2012 at 20:17Hi, Is there anyones out there using Sourcery CodeBench Lite for STM32F4xx? We've been using this one for STM32F10x series for a while. There is no problems for us untill we start using floating point instructions on...

npham by Associate II
  • 1694 Views
  • 3 replies
  • 0 kudos

UART connection

Posted on March 07, 2012 at 10:13I wanted touse theUART portbut can not findany informationto use this port,the portonly appears toUSART, does anyonecan give mesome tipshow you canconnect thestm32f4discoveryto establishcontact withthis type ofport (...

CUSTOMHID_SIZ_REPORT_DESC larger than 255

Posted on March 09, 2012 at 12:29I have a hid report created using descriptor tool 2.4. The final descriptor size is 289. which appears to be to large (hid not detected). If I cut a few reports out so the size becomes less than 256 it works fine. Is...

gurnett2 by Associate II
  • 1810 Views
  • 3 replies
  • 0 kudos

SDIO SD, Interrupt or DMA required.

Posted on March 09, 2012 at 20:36Hello,I have a question concerning SDIO driver provided by STM for the STM32F407.  Do you have to use interrupts or DMA?  Can you initialize the a SD Card and write data using:SDIO_SendCommand(&SDIO_CmdInitStructure)...

slagment by Associate II
  • 754 Views
  • 0 replies
  • 0 kudos

Reference power design for USB OTG host AND slave modes

Posted on March 08, 2012 at 16:35Hi Does ST have a reference design for an USB OTG use case where e.g STM32F4xx based board could be used both as a USB host providing 5V to the USB device and as a USB slave powering the whole board from the USB's 5v...

tuomas by Associate II
  • 1614 Views
  • 2 replies
  • 0 kudos

STM32VL with LCD

Posted on February 13, 2012 at 15:48Hello, Je suis un d�butant et j'essaye de commander une LCD (16 * 2) avec un STM32VL : afficher et ajuster une horloge (a l'aide des deux boutons B1 et B2 sur la carte) sur le LCD .et je sais pas par quoi je comme...

Troubles at receive more than one character (RTOS-RL-ARM)

Posted on March 02, 2012 at 12:34How to send and receive data using RTOS (RL-ARM) with tasks? (Without generating an interruption?) Using this functions below:TO SEND /*----------------------------------------------------------------------------   W...

esiqueira by Associate II
  • 1296 Views
  • 3 replies
  • 0 kudos

SWD Debugging multiple devices on one bus.

Posted on March 08, 2012 at 10:02According to this paper: http://www.arm.com/files/pdf/Low_Pin-Count_Debug_Interfaces_for_Multi-device_Systems.pdf, it is possible to use SWD to debug multiple chips that are all connected to the same debug lines. Acc...

mgerth by Associate
  • 1074 Views
  • 0 replies
  • 0 kudos

stm32f407 ADC data alignement problem -> solution

Posted on March 07, 2012 at 16:05I encountered a data alignement problem when using the 3 ADCs. ADC_Mode = ADC_TripleMode_RegSimult ADC_DataAlign = ADC_DataAlign_Right had no effect. Data was allways left-aligned. The Problem was that I omitted assi...

raffael by Associate II
  • 1021 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.