STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configuring input pull-up or pull-down

Posted on June 22, 2012 at 20:54Hi, I am using the STM32F103ZG device and looking through the reference manual (RM0008) I cannot find how, when a pin is configured as ''Input Pull-up/pull-down'', to select the pull-up or pull-down option. Having don...

dsjnews by Associate III
  • 3794 Views
  • 2 replies
  • 0 kudos

How to use the USB ISO IN Endpoint

Posted on June 21, 2012 at 09:40Hello.I have a probem with the ISO IN Endpoint. Double buffering is not working.The STM32F103RD is sending right data only from one buffer. Data from another buffer is wrong.My code:  /* Initialize Endpoint 1 */  SetE...

loginov by Associate
  • 989 Views
  • 1 replies
  • 0 kudos

SDcard with SDIO interface and FATFS

Posted on June 07, 2012 at 18:46Hello, i connected sdcard to my stm32f4discovery board, used SDIO example for low level init, and fixed fatfs so i can write data and read that later with computer But fatfs code is to complex for me to understand, do...

linas2 by Associate II
  • 5267 Views
  • 16 replies
  • 0 kudos

Timer using external clock nr 2

Posted on June 22, 2012 at 12:56  I'm using a STM32F103RBT6.Basicly I want to clock TIM1 (it should work on this frequency because of the Fmax from APB2) external with an 25.5 Mhz signal and use the Update_IRQ. Thats all.I can start TIM1 and use the...

ullmann by Associate
  • 7429 Views
  • 3 replies
  • 0 kudos

No Flash size register on STM32F2xx?

Posted on October 17, 2011 at 12:26STM32F2xx reference manual Doc ID 15403 Rev 3 doesn't list a Flash size register in chapter 33 Device electronic signature Is there really no such register? #missing-functionality

Unique device ID register address in STM32F2xx

Posted on June 11, 2012 at 13:45Hello, I’m trying to get the uID from a STM32F207 microcontroller using the integrated bootloader connected through the USART1 (as described in AN3155). I’ve already implemented this feature for other microcontrol...

PWM control with DMA and ADC

Posted on June 21, 2012 at 16:58The original post was too long to process during our migration. Please click on the attachment to read the original post.

esiqueira by Associate II
  • 1456 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.