STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

changing irq handler

Posted on October 25, 2012 at 16:17What is the best way to change the irqhandler to be used. I have a number of situations where the operations need to change depending on what the board is doing. Don't want to have a load of ifs or switches inside ...

gurnett2 by Associate II
  • 2629 Views
  • 4 replies
  • 0 kudos

low power STM32L speculation

Posted on October 25, 2012 at 16:25Hi. Erased state of flash memory in STM32L low-power devices is 0 instead of more common 1. What is the reason for this? If I will program unused flash portion to all FFh, will this impact current consumption in an...

jgoril2 by Associate II
  • 1119 Views
  • 1 replies
  • 0 kudos

SPI1 DMA channel/stream

Posted on October 25, 2012 at 14:38Where do I find out what DMA channel/stream i need to use for SPI1 TX.not sure which st document has this information in it?(stm32f4)Thanks :)

russdx by Associate II
  • 801 Views
  • 2 replies
  • 0 kudos

Flashing STM32F405 with ST link utility

Posted on October 24, 2012 at 21:07Hi all,After flashing my board based on a STM32F405RG with ST link utility (Hex compiled with GCC under eclipse), I can't communicate anymore with the core. I have this error :Cannot run core while booting from fla...

neoirto by Associate II
  • 2408 Views
  • 5 replies
  • 0 kudos

ST32f4discovery+sdcard+fatfs problem

Posted on June 30, 2012 at 23:43Hello, i have a small problem i think.With the help of this forum and google i created a project with CoIDE.What it should do is reading the directory of an SDCARD.The SDCARD part is working. but the fatfs is not work...

arnold by Associate II
  • 11466 Views
  • 48 replies
  • 0 kudos

Using CCM (or other ram) to store critical functions

Posted on October 23, 2012 at 13:50 Hi. I am using a STM32F4discoveryboard to prototype an application. In the application, I have some really critical interrupt that must be handled (or else there will be an uncontrolled surge of over 80...

marbel by Associate II
  • 3263 Views
  • 6 replies
  • 0 kudos

EOC interrupt for ADC

Posted on October 22, 2012 at 16:42  The original post was too long to process during our migration. Please click on the attachment to read the original post.

orn by Associate II
  • 6787 Views
  • 14 replies
  • 0 kudos

STM32F2 series flash mapping

Posted on October 24, 2012 at 19:51Hi,I am using STM32F207VE, and trying to perform read/write operation. Since this chip has flash memory of 512K, not sure how the mapping takes effect. Memory mapping is explained for 1MB flash, but not for lesser ...

mit by Associate II
  • 1249 Views
  • 2 replies
  • 0 kudos

STM32F2 series flash mapping

Posted on October 24, 2012 at 19:53Hi,I am using STM32F207VE, and trying to perform read/write operation. Since this chip has flash memory of 512K, not sure how the mapping takes effect. Memory mapping is explained for 1MB flash, but not for lesser ...

mit by Associate II
  • 774 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.