STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

iic with stm32f100

Posted on October 28, 2012 at 12:52Hello, i'm trying to access a compas modul with my stm32F100 (ST32VLDiscovery). I'm trying to do that directly accessing the registers. I think writing the data is ok, but reading doesn't work. I send the start, th...

EXTI on PC3 rising edge only : pull-down ?

Posted on November 07, 2012 at 12:53Hi all,One question about EXTI : I have to trigger an external interrupt on pin PC3 of my STM32F405RG.So I have to configure EXTI3 for rising edge, but is it a good practice to enable pull down to avoid false trig...

neoirto by Associate II
  • 728 Views
  • 0 replies
  • 0 kudos

CAN BUS

Posted on November 06, 2012 at 13:12Hi,I was looking for an example of a CAN BUS for STM32F4 can you help?

orn by Associate II
  • 1459 Views
  • 3 replies
  • 0 kudos

STM32 communicate with MIPI RFFE interface.

Posted on November 05, 2012 at 23:47I am thining of to use STM32 to communicate with MIPI interface. Please see the typical format in the attachment. It is hard to do that with PIC18F controller, for data rate up to 26MHz; by-directional TX/RX SPI l...

Unable to set OVER8 in STM3240G-EVAL (STM32F407IGH6)

Posted on November 05, 2012 at 08:21Hello Friends, Am trying to achieve a high baud rate using USART1 - 7.3728Mbps SYSCLK=168MHz APB2=84MHz Now to achieve this baud rate, I need the OVER8=1 (3 bits for Fraction) Using example code, I set the OVER8 b...

Bootloader version

Posted on November 05, 2012 at 15:09Hello, I have these information written on the stm32f105 micrcontroller STM32F105 VCT6        Z 990TD   93 MYS 99 045 I have read that it depends on the date code of the microcontroller which is 045 in my case. Wh...

hisham23 by Associate III
  • 2959 Views
  • 6 replies
  • 0 kudos

LIS3DH g-sensor read byte problem

Posted on November 06, 2012 at 13:35hi all, i am working on LIS3DH acc. with stm32f100c8.i read WHO AM I byte(0x33) but i cannot read z axis value(2Dh)..please any suggestions? here is my read one byte funct.slaveAddress 0x32ReadAddr 0x2D //z axis v...

Timer output toggle issue

Posted on October 25, 2011 at 20:02Hi all,I have a strange problem using Timer1 in Output Toggle mode. My objective is to generate square waves of different frequencies using the same timer. I've based my code on the 'TIM_OCToggle' example in the St...

need some project advice :)

Posted on October 07, 2012 at 14:21Hello :)I have a little project using a stm32f4 which receives usb data from the pc using the cdc classes (2048bytes @ 60fps) and then draws them to a Plasma dot matrix display.I have it all working ok :) The probl...

russdx by Associate II
  • 2919 Views
  • 13 replies
  • 0 kudos

STM32F2xx and STM32F4xx Demonstration Builder Compile

Posted on November 02, 2012 at 18:18I am having difficulty compiling the Demonstration Builder example code.  I am using MDK-ARM (Keil) with the 256k license but the code is 265k when linked.  I read the app note to disable modules but when I tried ...

wmoyne by Associate II
  • 1564 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.