STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f4 discovery n00b/debug question

Posted on November 18, 2012 at 15:55Sorry if this is a repost that I missed but I'm looking to play with one of these boards to practice porting RTOS's to such as uCOS II/III.  But I don't know much about the debug capabilities provided by STLINK/V2...

pauls931 by Associate
  • 2365 Views
  • 4 replies
  • 0 kudos

Remap ADC

Posted on November 17, 2012 at 16:54Hi,Maybe a dumb question but....Would it be possible to remap like 6 inputs of ADC1 to other pins? (stm32f4discovery)I just found some info regarding the remapping of can etc. and i couldn't find theinfo for ADC1....

kenny__84 by Associate II
  • 2481 Views
  • 4 replies
  • 0 kudos

printf and sprintf why it should not be used?

Posted on November 17, 2012 at 12:09To print the result of the ADC on my LCD (16x2) I use the following actions:sprintf(Sprint,''%d'',ADC3ConvertedValue[0]);LCD_PrintData(Sprint, lenght(Sprint)); //  length (Sprint) returns the size of the carrier S...

orn by Associate II
  • 4115 Views
  • 3 replies
  • 0 kudos

STM32F4 Pins and Modules Configure software

Posted on November 17, 2012 at 06:38STM32F4?????????,?????C????. Functions: 1 Pins assignment and  pins confliction indication. 2 making ''C'' program for all modules. Future functions: 3 make program for other modules, eg, watchdog  module,DMA modu...

Problem with stm32f100c6 clock configuration

Posted on July 16, 2012 at 19:50Hi everybody! I'm using STM32F100C6 with IAR Embedded Workbench IDE and i'm trying to configure the system clock. First i tried to use the external oscillator HSE that's built on the board, 20MHz, here's the code rela...

Discovery-F3 and Discovery-F4 Difference Articles

Posted on November 17, 2012 at 00:13I have written two articles that you may find helpful if you are trying to decide between the STM32 F3 or F4 microcontrollers for a project. Or between the Discovery-F3 and the Discovery-F4 modules. The first arti...

kornak by Associate II
  • 3224 Views
  • 0 replies
  • 0 kudos

Storing image and wave file on SD card

Posted on November 16, 2012 at 06:06How to store image or wav file on SD card (without using FATFS) ...i m using SDIO interface, Keil development environment and discovery board I m done with sd card initialization and single block read write functi...

aambreen by Associate II
  • 749 Views
  • 0 replies
  • 0 kudos

stm32 link utility: core is held in reset

Posted on November 15, 2012 at 18:53First i had problems with the ST-Link drivers, then I had success with installing them. Now I get ''core is held in reset'' error in st-link utility.How to fix this? My only idea is that I shorted something when I...

blaz by Associate
  • 1522 Views
  • 1 replies
  • 0 kudos

Stuck in IRQ handler mode under GDB ? (STM32L152-EVAL)

Posted on November 15, 2012 at 19:33Hello,I am new to debugging on the STM32 and I have a STM32L152-EVAL board and I am trying to bring up the new open source version of RTX on this board.  My setup is as follows.This is setup on a Mac running Mount...

jack23 by Associate
  • 865 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.