STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

usb problem

Posted on February 05, 2013 at 14:06The original post was too long to process during our migration. Please click on the attachment to read the original post.

marwa2 by Associate II
  • 862 Views
  • 1 replies
  • 0 kudos

Unable to send data via UART Serial Link

Posted on February 07, 2013 at 05:12I am trying to send data to a PC COM port but cannot figure it outI configured GPIO, NVIC, and USART per specification and it all checks out. The strange thing is, when I connect the Tx pin and ground to oscillosc...

skillet by Associate II
  • 3375 Views
  • 7 replies
  • 0 kudos

STM32F103ZC LQFP144 Programming Problem !

Posted on February 07, 2013 at 13:22Hi ,I have two development board which is the first have stm32f103vg LQFP100and second have stm32f103zc LQFP144 I can program LQFP100 model microcontroller using default SWD settings , but at the LQFP144  model i ...

From IRQChannel to IRCHandler

Posted on February 06, 2013 at 02:21Hello guys,when I initialize for example this Interrupt:NVIC_InitStructure.NVIC_IRQChannel = OTG_FS_IRQn;  I suppose it will have OTG_FS_IRQHandler as it's handler, but where can i look this up? I already searched...

How to reset virtual COM port driver?

Posted on February 06, 2013 at 18:37Hi, i am using the VCP for communication between a PC software an my STM32F207 device. Works ok so far. But if the device restarts while the PC software maintains the connection (or if somebody pulls out the cable...

zabel by Associate III
  • 958 Views
  • 0 replies
  • 0 kudos

Fast gpio read with sync

Posted on February 05, 2013 at 09:46Hello, I have 16b parallel bus, 8MHz adc, and I need to read as fast as I can data to memory array which is 128 point long. So far I overclocked stm32f4 to 250MHz so I could do it faster. Original code is :while(i...

linas2 by Associate II
  • 2013 Views
  • 4 replies
  • 0 kudos

6 CH PWM on TIM1 (What is Wrong with my Code)

Posted on February 06, 2013 at 11:09 Hello, I am currently migrating from Microchip MIP to ST ARM Cortex M3 so I am new to Cortex M3.I have been trying for days to configure Advance TIM1 in STM32F103RB to output 6 Channel PWM but it has prove to be ...

STM32L Stop Mode

Posted on February 05, 2013 at 20:46I cannot get stop mode current below 1.1 mA in the IAR STM32L152VB eval board. This is the code to prep and then go to stop mode:lowPowerConfigGPIO();  (this configures all GPIO pins as ADC inputs)PWR_FastWakeUpCm...

Understanding RCC register

Posted on February 05, 2013 at 15:05I'm trying to understand how below function call  from usb_bsp.c source file works:RCC_APB1PeriphResetCmd( RCC_APB1Periph_PWR, ENABLE );This is from Reference Manual:5.3.8 RCC APB1 peripheral reset register (RCC_A...

dimax by Senior
  • 2108 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.