STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Brusless motor with ESC's

Posted on February 21, 2013 at 16:52Hi to everyone,I have a brushless motor 850Kv and one ESC's . The main aim of my task is to control my motor (forward and backward)  by setting in different speeds. The microcontroller which i have is the STM32F4 ...

STM32f0 SPI trouble

Posted on February 24, 2013 at 02:04I am using the stm32f0 discovery board and having trouble getting SPI to talk properly with an external SPI sensor. As a test case, I wrote a small program to send bytes from SPI1 to SPI2 and then compare these se...

USART DMA questions

Posted on February 21, 2013 at 22:48Hi, I am having a hard time to make USART RX work in DMA mode. I am using SMT32F103, just want USART2 to communicate with serial monitoring software like hyperterminal... I have had USART2 TX working in core drivn...

romey by Associate II
  • 2854 Views
  • 5 replies
  • 0 kudos

Clearing the OCxREF signal on an external event

Posted on February 14, 2013 at 14:30Hello.As described on STM32F100 manual:The OCxREF signal for a given channel can be driven Low by applying a High level to the ETRF input (OCxCE enable bit of the corresponding TIMx_CCMRx register set to ‘1’)....

casainho by Associate II
  • 3208 Views
  • 6 replies
  • 0 kudos

measure the duration of a loop ?

Posted on February 22, 2013 at 11:20Hi Can I measure the duration of a loop in the program of STM32F4 using TIMER ? For example ______________________________________ Begin (Timer x) For (;;) //infinite loop { .... ... ... .. } End (Timer x) ...

bmwael1 by Associate II
  • 2271 Views
  • 5 replies
  • 0 kudos

TIM14 @ STM32F103VGT6

Posted on February 22, 2013 at 18:10Hi, I would like to use TIM14 @ STM32F103VGT6 uC but it doesn't defined everywhere. Did anybody used this timer before? What was the startup file used? Best regards, #stm32-tim14-stm32f103vgt6

gsilva by Associate II
  • 1502 Views
  • 2 replies
  • 0 kudos

STM32F103RBT6 development board + 2.8'' TFT-module

Posted on June 25, 2011 at 19:59Hey people, Recently I bought the STM32F103RBT6 development board + 2.8'' TFT-module. (A.k.a MINI-STM32-V3.0) (with the 2 mini USBs) After many attempts to enter programming mode, and program it via USB without any ...

UART initialisation

Posted on February 22, 2013 at 09:24Hi everybody,I'm using a STM32F205VE and something that I don't understand.I do this :  USART_InitStructure.USART_BaudRate = 9600;  USART_InitStructure.USART_WordLength = USART_WordLength_8b;  USART_InitStructure....

STM32 CAN Receive Mailbox

Posted on February 20, 2013 at 13:40Hi,I am working with STM32F101 using CAN1 controller.I configure the CAN filter to accept messages from 0x100 to 0x1FF as follows:CAN_FilterInitTypeDef CAN_FilterInitStructure ; CAN_FilterInitStructure. CAN_Filte...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.