STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

usart + sd card interaction

Posted on March 05, 2013 at 14:36Hi, I am using STM3240G-Eval , i know that in this evaluation board MicroSD Card shares I/Os with motor control, RS-232 and audio . So i am trying to work around this limitation. I have the following flow : initUSART...

stm32f4 discovery and dac

Posted on March 05, 2013 at 14:19hey there,recently I've started playing with a stm32f4discovery with the final goal of realizing the control of a particular simple device we had in our company. It is my first embedded project so I'm quite new to th...

multi ADC and DMA ==> memory problem

Posted on March 05, 2013 at 16:57Hello, I need to measure 3 ADC channels in continuous, I use the STM32L151VB. I use the DMA transfert, my firmware doesn't work property. please see in attachment my source code my problem is the  memory data  ''adcB...

willdu87 by Associate
  • 1197 Views
  • 2 replies
  • 0 kudos

STM32F051 possible missconfig? makes Battery pin takes 100mA

Posted on March 05, 2013 at 15:57Hi, I have a STM32F051C6 on a PCB that has a socket for a Battery, connected to VBat using a Schottky diode. While development phase I don't fit the battery, just use a jumper wire and connect the Plus of the battery...

jgnoss by Associate III
  • 4261 Views
  • 8 replies
  • 0 kudos

usb library patch

Posted on January 09, 2012 at 10:47Hi, where can I submit usb library patch(es)? #stm32 #bluetooth

spam by Associate II
  • 2395 Views
  • 5 replies
  • 0 kudos

understanding i2c signal

Posted on March 05, 2013 at 12:16Hi, I am programming the STM3241G-EVAL to work as a i2c slave to comunicate with a mother board running Linux. In the tests I am using the linux i2c-tools.When I try to send a byte (0x35) to the device address (0x0A)...

0690X000006053YQAQ.png
occam25 by Associate II
  • 2265 Views
  • 3 replies
  • 0 kudos

Broken link on ST-website for STM32 resources

Posted on March 05, 2013 at 17:20Hello,    I was trying to get the ST-LINK software and drivers for the STM32 board. The links provided seem to be broken.  Google, in addition to the forum posts of days past, point me to these links:http://www.st.co...

STM32f407vg discovery cannot communicate with ST link

Posted on July 18, 2012 at 16:51it shows like:Error : Cannot communicate with the device !Check the SWD cable connection and check all the needed pin connections on the SWD connector.Reboot the ST-Link with USB cable.If the device has been programme...

vinothraj by Associate II
  • 5310 Views
  • 14 replies
  • 0 kudos

remove protection level 1

Posted on March 05, 2013 at 17:05 hey , i was testing the flash driver of stm32f407vg. and during the testing of the option bytes i set the rdp of the flash to protection level 1. since then all debugging facilities have been disabled. even the f...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.