STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 discovery

Posted on March 10, 2013 at 08:28Hi all I am new to this STM32discovery  board. I need help to find the right functions that will  initiate any chosen header pin to INPUT or OUTPUT or PWM  or A/D when relevant . Where exactly I find those funct...

STM WAKE UP

Posted on March 10, 2013 at 19:41Its time to upgrade to an easy to implement forum like those http://www.picaxeforum.co.uk/forum.php http://arduino.cc/forum/ The STM boards give a real via delaroza when new to them .  The information to new users i...

how to make a delay on STM32

Posted on March 07, 2013 at 15:01Hello!how to make a delay of N clock cycles? (without timers)I realized asm(NOP) is not working

maryuriy by Associate II
  • 2666 Views
  • 5 replies
  • 0 kudos

90 degrees phase difference signals

Posted on March 11, 2013 at 11:05I want to create 2 signals and they must have 90 degrees phase difference (on square wave). for example signals have 2 kHz freq. i set the timer 8 kHz and just changed the one of the outputs on each timer interrupt. ...

ADC preventing SysTick timer Interrupt (Why?)

Posted on March 10, 2013 at 17:56Hello, Once I initailize ADC in my program, it stop the SysTick timer Interrupt from working while ADC work correctly.I want ADC Interrutp to have higher priority than SysTick timer Interrupt.How do I set the priorit...

HMAC with DMA transfert

Posted on March 09, 2013 at 14:40The original post was too long to process during our migration. Please click on the attachment to read the original post.

JTAG unable to attach to CPU

Posted on March 08, 2013 at 22:24Hello ST community, first forum post... We're having problems with downloading EVAL example code into STM32F207ZC. I've soldered 144-pin chip to an adapterboard and followed schematics in AN3320 ''Getting started wit...

optifier by Associate II
  • 3321 Views
  • 7 replies
  • 0 kudos

bootload from a pc program

Posted on March 07, 2013 at 00:35Hi all i have to write an interface program for write to the stm32f40x's flash. I did a control system but users want to change some parameters on program but i can't give them the sources. I must write bootloader pr...

problem with USART multi-processor mode

Posted on March 06, 2013 at 08:33Dear,    I met the problem when use the USART multiprocessor mode. In my USART communication application, even for one USART, there are 3 different addressses for different data packages. But STM32F4 only provide one...

xinjin by Associate II
  • 3901 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.