STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 BOOT

Posted on March 14, 2013 at 16:09 Hi, I got the a problem regarding the BOOT process, I don't know how to move the nBOOT1 pin.  I have tried via software with the FLASH functions but with no good result.  Also I am working with the J-link no with...

giorgio2 by Associate II
  • 718 Views
  • 0 replies
  • 0 kudos

USB dual profile

Posted on March 13, 2013 at 22:23Hi, I have a project with a STM32F205 and I was wondering if I can have two USB profile loaded. I want to have the ''mass storage'' profile as well as the ''HID''. Is it possible? My second question is regarding the ...

jbaron by Associate
  • 947 Views
  • 1 replies
  • 0 kudos

EXTI signal capture speed limitation

Posted on January 18, 2013 at 15:12 Hi all, I am using a DiscoreryF4 board to develop a small application that counts pulses entering a specific pin. This is required to read the pulses from a field instrument that generates the pulses as...

hermanv by Associate II
  • 5693 Views
  • 10 replies
  • 0 kudos

USB FLASH STICK

Posted on March 14, 2013 at 10:50Hello In my new project I need to connect 2 or 3 USB sticks to stm32f4 ; later on i was able to do that with one stick only ; is that possible ? Could you suggest me a solution ? Regards

sami by Associate II
  • 941 Views
  • 1 replies
  • 0 kudos

Debouncing interrupts

Posted on March 10, 2013 at 23:38Hi, In our system, we are trying to debounce switches on GPIO lines. Every msec the switch is sampled using TIM3. After 16 ticks, if the input has settled, the idea is to set the interrupt pending register and trigge...

stenasc by Senior
  • 6081 Views
  • 14 replies
  • 0 kudos

Can't start application without debugger

Posted on March 13, 2013 at 09:05Hi everyone!I haven't found any useful information about my trouble, unfortunately. I am a newbie in STM32 MCUs. But I've used another ARM-based devices before.I've started with STM32F102R8. Using IAR and ST's periph...

stm32f10tvct uart5

Posted on March 08, 2013 at 10:46hi, I'm working with the stm3210c_eval and I would like to use the UART5 . this is the configuration void UART5_Init(void) {   GPIO_InitTypeDef GPIO_InitStructure;   USART_InitTypeDef USART_InitStructure;   /* Clock...

aymen by Associate II
  • 1770 Views
  • 5 replies
  • 0 kudos

STM32 USART Timing problem

Posted on March 11, 2013 at 13:07Hello; i have a small USART Test application.  It should send, controlled by an timer, constant ''A'' characters By receiving a character from the terminal Program of the PC an interupt is fired. The terminal program...

mrupprath by Associate II
  • 1484 Views
  • 3 replies
  • 0 kudos

SPI3 not working

Posted on September 05, 2012 at 21:45 Hello, ai am trying to comunicate with external DAC and having some hard time using SPI3 in GPIOC port (12,10 and 11 for CS) i have no problem with SPI2, but SPI2 is for LCD touschreen so i want to make new...

linas2 by Associate II
  • 1129 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.