STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-link program problem

Posted on April 08, 2013 at 04:00Dear,    I sucessfully download the Custom_HID demo code on STM32L152-EVAL. It works. However, after I disconnect the USB cable from CN1, I use IAR and ST-link to program again, the error ''Fatal error: Failed to rea...

xinjin by Associate II
  • 2271 Views
  • 4 replies
  • 0 kudos

keil USB host with ST standard library

Posted on March 23, 2013 at 11:52Hi I am trying to create a USB host project with keil library (USB HOST and FILE system) + ST standard library ; I always get the error OTG_HS_DFIFO  Not found ... those fifos are defined in STM32F4XXH in keil bu...

sami by Associate II
  • 1624 Views
  • 3 replies
  • 0 kudos

STM32F4Discovery simple timer for delay

Posted on April 04, 2013 at 20:11I have problems with creation of simple timer for delay. For a week I am searching some code examples where timers will working without interrupts, examples are working but not quit correct. One of examples http://am...

raimondas by Associate II
  • 3310 Views
  • 6 replies
  • 0 kudos

STM32F429/STM32F439: Possibly with internal USB-HS?

Posted on April 06, 2013 at 12:17Hi, concerning the new STM32F429/STM32F439 chips: In the part number table in column ''Serial interface'' it says ''2xUSB OTG FS/HS'' for most of them - whereas for the older chips (as STM32F407...) it says ''2xUSB O...

flyer31 by Senior
  • 1316 Views
  • 2 replies
  • 0 kudos

2 APP with IAP

Posted on April 07, 2013 at 00:26Hello.If I want tosave 2 FW (current one and newer) on 2 section. This is for robust cases when I want to be sure I have a good update FW before delete the old one.For that I made 2 sections (let say section 3-6 for ...

Barbie by Associate II
  • 1477 Views
  • 3 replies
  • 0 kudos

ST-Link/V2 Dead, isn't detected by any PC ! :) Please help..

Posted on April 05, 2013 at 10:12Hi everybody, After receiving the board and installing the kit from Keil plus1 hour of struggling with set-up the board was ok :), ran some examples. Ok, excellent, reflashed the ST Link with the new firmware using t...

petre by Associate II
  • 3041 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.