STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeRtos ARM

Posted on April 16, 2013 at 15:15Does someone know where can i find a tutorial about configuring a FreeRTOS ARM Cortex-M4F demo application that targets an STMicroelectronics STM32F40XX microcontroller using eclipse please ? http://www.st.com/intern...

ST LINK error

Posted on April 17, 2013 at 08:53Since yesterday, i can't establish a ST LINK connection with my STM32L1-Discovery board. I've tried it in CrossWorks on my MacBook, the error was 'ST-LINK LOG'. After that, I've tried it on my windows 7 pc with ST LI...

USART ore after 8 bytes always

Posted on December 28, 2012 at 01:21 Hello All, I'm sending data over a bluetooth device to the stm32 discovery board on usart 2. Everything is great unless I send a large amount of data (80 bytes). If I send this large amount I only end up ...

STANDBY and RTC

Posted on April 15, 2013 at 15:14Hi Again ; In my application stm32f407 will enter stanfby mode then should wake up by 2 methods ; a rising edge on the PA0( wakeup _pin) and an alarm occurs everyday one time .. the first one I thing I will not get...

sami by Associate II
  • 3719 Views
  • 9 replies
  • 0 kudos

STM32F2xx start program not from 0x08000000

Posted on April 16, 2013 at 08:37Hello. Can I put my program start from diffrent address then 0x08000000 ? I have same data sector I need and because I can't know the size of my program I want to make it this way: Sector 0-1 will be for data. My pro...

Barbie by Associate II
  • 1780 Views
  • 3 replies
  • 0 kudos

STM32F4 FreeRTOS task and SPI interrupt problem

Posted on April 16, 2013 at 12:04 Hi,I am working on a project with STM32F4 and FreeRTOS. I have a SPI ISR for receiving data from SPI in the speed of about 5Mbps, I also have a task which handles those data. The Queue is used to be between the i...

Changing frequency in PWM

Posted on February 12, 2013 at 06:19Hi All I am using TIM2 for generating a pattern of pulses like pulse with 30 % duty cycle followed by pulse with 40% duty cycle and 50% duty cycle. I am able to generate it however I am not able to get the accurac...

sajeed by Associate II
  • 1270 Views
  • 1 replies
  • 0 kudos

EXTI configuration to different lines

Posted on April 16, 2013 at 14:11Hi, I encounter to some problem in understanding of correct EXTI configuration. From ST example and RM0090 Figure.27  I understood that each Pin_0 (A,B...I) connects to EXTI0 interrupt, Pin_1 (A,B...I) to EXTI1 and s...

vault by Associate
  • 1220 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.