STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 FSMC synchronous burst AHB size?

Posted on April 30, 2013 at 11:02Hi.I have a problem with FMSC. I want to use FSMC single synchronous burst transfer with PSRAM. The memory has a 16bit data width and i read into ref. manual that ''When the selected bank is configured in synchronous...

slqa123 by Associate
  • 1596 Views
  • 2 replies
  • 0 kudos

STM32F4 RTC Alarm problem

Posted on April 28, 2013 at 23:08 Hello I am trying to setup he alarim to wakeup my MCU from standby everyday at 12:00 but it seems that some times the alarm nor occurs and some it occurs .. what i miss in my code? RTC_AlarmCmd(RTC_Al...

sami by Associate II
  • 1521 Views
  • 4 replies
  • 0 kudos

Capteur Internal Temperature sensor..!!

Posted on April 27, 2013 at 00:26HiI find problems with capateur internal temperature sensor STM32F4 Discovery, I have measured as false (-80.50...-45.00...-60.50 ).I know if my code is wrong or the formula that calculates the temperature.I hope the...

MEMS accelerometer measures

Posted on April 26, 2013 at 18:25HI, I want to know how to convert the values ​​that provides MEMS accelerometer on  g  because I need to set the threshold for single /double click detect.For example in the program MEMS in STM32F4-Discovery_FW_V...

karoui by Associate II
  • 2181 Views
  • 4 replies
  • 0 kudos

What am I missing? ADC again...

Posted on April 27, 2013 at 13:07Hi all, I've the following problem. I need to measure signal on the PC.00 pin and with the code bellow it doesn't work. :( However, if I change the pin to PC.02 and Channel 12 , everything works fine and I get the pr...

jamsoft by Associate II
  • 4281 Views
  • 10 replies
  • 0 kudos

rs485 Communication through usart

Posted on April 27, 2013 at 08:12I am using stm32f107rc for rs485 communication through usart1 and usart3. i am receving a set data from usart1 to an array and trying to transmit the same set of data from an array through an usart3. it works fine fo...

aru by Associate II
  • 1767 Views
  • 3 replies
  • 0 kudos

DMA request from external input signal

Posted on April 16, 2013 at 12:40I have an input 8 bits parallel bus, with a CLK signal connected to GPIOs. The frequency is 1MHz. I need to configure an automatic DMA transfert from the 8 bits GPIO to a memory buffer (dual buffer mode would be grea...

USART RX - HOW IT WORKS ?

Posted on April 19, 2013 at 16:43 Hello, I'm quite a newbie with USART RX, I read a lot of code examples but I don't exactly understand how it works. I want to receive MIDI data from a musical instrument. MIDI is a protocol using USART c...

ADC data corruptiom

Posted on April 25, 2013 at 10:53The original post was too long to process during our migration. Please click on the attachment to read the original post.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.