STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer 5 Setup

Posted on May 28, 2013 at 22:49I'm just stering with the STM324f Discovery board and am trying to get timer 5 setup as a free running 1us timer that I can access in my code for timing. No matter what I do, I can't get TIM5->CNT to change from zero. ...

cwparker by Associate II
  • 1126 Views
  • 1 replies
  • 0 kudos

How to set RTC Alarm in stm32

Posted on May 28, 2013 at 14:15Hi! All,I want to set RTC alarm for specific date and time can any one help me in this regard? i use STM32l151vbt6.Thank You, #stm32l1-rtc-alarm

AN3309 xls file

Posted on May 28, 2013 at 13:29Hello, Can someone please tell me where i can found the STM32L1xx_Clock_Configuration_VX.Y.Z.xls that the AN3309 talk about ? Thanks. #an3309-clock-configuration

nicolas by Senior II
  • 1269 Views
  • 2 replies
  • 0 kudos

Delay Function Without SysTick_Handler Interrupt

Posted on May 27, 2013 at 15:58Hello , I want to try use a function that is without  SysTick_Handler Interrupt : I wrote this function  : void DelayUs(int us) { unsigned int cnt; while(us-- >0) {    cnt = SysTick_GetCounter(); // get systick count...

Java binary

Posted on May 07, 2013 at 16:41Hi,Resulting  binary can be downloaded to a general STM32  or only to a Java enabled one?

5V & 3V3 POWER SUPPLY BAT60 DIODES: are they critical ?

Posted on May 20, 2013 at 12:11Hello,I'm currently designing my own schematic based on the STM32F4DISCOVERY board.The two BAT60 power supply protection diodes (D1 & D3) are not relevant for me because they generate a dropout voltage: +5V is in fact ...

STM32F4 with external NAND-Flash - whats the Adress Area?

Posted on May 28, 2013 at 01:00Hi, I'm using this Board: http://www.keil.com/support/man/docs/mcbstm32f200/mcbstm32f200_to_memory.htm to build up a small webserver interface. I want to put the website data on the NAND-Flash. But what is the Adress o...

sam239955 by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

adding USB interface descriptor

Posted on May 26, 2013 at 19:53The original post was too long to process during our migration. Please click on the attachment to read the original post.

stm32 by Associate
  • 1152 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.