STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Comparitor interrupt on STM32L151?

Posted on June 12, 2013 at 13:45Hi all, I'm using a STM32L151VCT6. I was hoping to make use of the internal interupt associated with Comparitor 2 (EXTI 22). On further inspection, I've noticed the Reference Manual (RM0038) shows two block diagrams ...

emily by Associate
  • 1402 Views
  • 2 replies
  • 0 kudos

I2C DMA data sizes

Posted on June 11, 2013 at 21:12 Using a STM32L152RB I'm trying to send some data out on the I2C bus using DMA, but I can't quite get the data to transmit like I expected. This is how I'm initializing the DMA. My memory source is...

kevin by Associate II
  • 1896 Views
  • 3 replies
  • 0 kudos

STM32F103CBT6 CPAL I2C freezing main loop

Posted on May 15, 2013 at 17:36Hi all, I have been using the CPAL I2C library on a STM32F103RBT6 to communicate with an external device which works fine. I have run the same code on a target board containing a STM32F103CBT6, I2C1 is used so I have n...

Measuring pulses on different pins

Posted on June 13, 2013 at 11:43Hello,I am trying to measure the time between the falling edge of a pulse on one pin and the falling edge of another pulse on another pin. I am trying to do it on TIM2 channel 2 and channel 3 on an STM32F0 discovery. ...

dstanton by Associate
  • 1026 Views
  • 1 replies
  • 0 kudos

Timer Interrupt STM32F4

Posted on June 13, 2013 at 05:44I'm having difficulty getting a simple timer reload interupt system to work. Once the initTimer() method is called the MCU appears to stop.  Even when I comment out ''soloInd->flash();'' Any help at all would be much ...

wkanew by Associate
  • 1155 Views
  • 2 replies
  • 0 kudos

STM32f4 discovery with touch screen

Posted on June 11, 2013 at 12:03hello ! can i use this TFT to interface with my board? this is the link to that TFT http://harizanov.com/2013/02/1-8-tft-lcd-display-on-raspberry-pi/img_1913/

keypad 4*4 with STM32* GPIOA

Posted on April 05, 2012 at 13:03salut, svp jr veux interfacer une clavier 4*4 avec un stm32 par les GPIO.... comment!!svp !!! NB : je met les 4 premier pins en 1     GPIO_SetBits(GPIOA,GPIO_Pin_0);           GPIO_SetBits(GPIOA,GPIO_Pin_1);         ...

eCos RTOS ported to STM32F4-Discovery board

Posted on June 12, 2013 at 20:56The free and open source eCos RTOS has been ported to the STM32F4-Discovery board. Details at:http://ecos.sourceware.org John Dallaway #ecos-rtos

jld by Associate
  • 960 Views
  • 0 replies
  • 0 kudos

STM32F407VG - write protection after power supply failure

Posted on June 12, 2013 at 18:01After power supply failure the processor is locked for writing. I've tried many ways to solve this, but with no result.Processor refuses programming. Every attempt to change ''Option bytes'' with st-link utility finis...

krolik by Associate
  • 1039 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.