STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UDIS/ URS - Bit, stm32F3

Posted on September 16, 2013 at 20:54Hello my dear Forumers,I'm having difficulties to understand the Update Disable bit and Update Request bit.In the peripherial libs it is said, and i quote:Configures the TIMx Update Request Interrupt source.  * @...

Core reset without peripheral reset

Posted on September 13, 2013 at 15:37Hi forum!I am trying to launch a soft reset of the STM32F417 core without losing peripheral state or resetting the peripheral registers. I intend to jump from one application (in flash) to another (in SRAM), for ...

slal by Associate III
  • 4568 Views
  • 8 replies
  • 0 kudos

STM32F4 Timer2 off - Pin status problem

Posted on September 12, 2013 at 23:49Hello, I have problems to set up the right pin state while TIM2 is configured in PWM mode and turned off. The corresponding CC output pin stays HIGH while timer is off but I strongly need it to be LOW. I thought ...

totally by Associate II
  • 1732 Views
  • 4 replies
  • 0 kudos

Coocox and the stm32f427vit6

Posted on September 12, 2013 at 11:33Hello,I was using Coocox and the STM32F407VGT6 and now I move to the new STM32F427VIT6. This microcontroller is not supported by Coocox, I have to select I'm using a STM32F407 but it works with that config (I can...

When I touch the SCL pin with my finger the SPI works

Posted on September 11, 2013 at 17:32Hello,I programmed a LCD screen with SPI on a prototype and everything was working fine. But I mounted the screen on the final PCB and now I have a problem: the screen didn't understand the datas I send to it. Th...

J-Link and STM32F103VET6 issue

Posted on September 15, 2013 at 01:18Guys I got : Guys, I got error on reading STM32 : What should I fix ? thanks **JLink Warning: Identified core does not match configuration. (Found: None, Configured: Cortex-M3) * JLink Info: TotalIRLen = 9, IRPri...

Startup file and interrupts

Posted on September 14, 2013 at 21:34  The original post was too long to process during our migration. Please click on the attachment to read the original post.

eltar by Associate III
  • 2070 Views
  • 2 replies
  • 0 kudos

Help with SDIO

Posted on March 04, 2013 at 18:09Hi guys. First of all, sorry if my english is bad. I have a problem configuring a uSD and SDIO port. I'm using the ST SDIO example for STM32f4 discovery board and I cant comunicate with de micro SD. I checked the pin...

STM3240G-EVAL Help me please!

Posted on October 06, 2012 at 11:50Hi, I just bought an evaluation board STM3240G-EVALI tried to modify the example provided by ST called ''ADC3_DMA'' but I could not change the pin from what I acquire the signal For example I wanted to go from pin ...

fullcaos by Associate II
  • 6611 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.