STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Partial Alternate Function mapping

Posted on October 08, 2013 at 23:35what is difference between  two ''Partial Alternate Function mapping'' and ''Full Alternate Function mapping'' for @param in GPIO_PinRemapConfig() on stm32f10x_gpio.c driver?thank you #partial

_behn4m by Associate II
  • 1167 Views
  • 2 replies
  • 0 kudos

stm3210C-Eval Debug-HSEStatus

Posted on October 07, 2013 at 08:59hello forum. I am new at arm so first I want to use the GPIO. I use stm3210c-eval. and this development board use stm32f107VC. I write code like this.#include ''stm32f10x.h''#include ''stm32_eval.h''#include <stdio...

RTC of STM32F1 wakes up from STOP after 1 sec

Posted on October 08, 2013 at 18:29 Hi all, I use RTC_IT_ALR of STM32F102 to wake up from stop mode. In my IRQ Handler, I do this : RTC_SetAlarm(RTC_GetCounter()+ 10); and in main : while(1){ PWR_EnterSTOPMode(PWR_Regu...

Kuikui by Associate III
  • 694 Views
  • 0 replies
  • 0 kudos

Running code from RAM

Posted on September 16, 2013 at 22:20Hi all!I am wondering if anyone has tried jumping from flash code to an entire project in internal SRAM without resetting (so no memory remap / boot0/boot1 config is required). I am working on the STM32F417, and ...

slal by Associate III
  • 7060 Views
  • 14 replies
  • 1 kudos

JTAG vs Serial Wire

Posted on May 13, 2013 at 19:46I'm using the STM32F407 in a new design and due to a conflict of peripheral pin assignments (Why isnt there more clk pin assignment flexibility?) I cannot use the JTDO pin of the device for JTAG. I think my only option...

Flash Memory: crash on write access

Posted on October 07, 2013 at 18:11 Hi I'm trying to write to the Flash ROM on my STM32F3 board (256k). Erasing a page works fine, but when I try to write a word (or half word), the MCU crashes. I'm doing what the standard peripheral l...

stm32L discovery onboard st-link

Posted on October 06, 2013 at 23:12Hi, I've got a question about using ST-LINK/V2 to program/debug an external application: if onboard st-link can be used only for MCUs from STM32L1 series or from other series too? I'm asking because in UM1079 it is...

kkkuba by Associate II
  • 1707 Views
  • 3 replies
  • 0 kudos

STM32F205 Flash Programming

Posted on October 18, 2012 at 20:11To erase a sector, follow the procedure below:1. Check that no Flash memory operation is ongoing by checking the BSY bit in the FLASH_SR register2. Set the SER bit and select the sector (out of the 12 sectors in th...

ramv by Associate II
  • 3042 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.