STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TFT+ SSD1963

Posted on October 29, 2013 at 22:52helloMy question is this .... I'm working on a project that involves a WF57BTIBCDC Winstar TFT (SSD1963 controller, 8 bit) with Dyscovery STM32F4. my question is: I need an external memory to work with FSMC compuls...

STM32F3 Vbat monitoring problem

Posted on October 30, 2013 at 11:57 Hello. STM32F373C8, IAR I have a problem with monitoring battary charge on Vbat pin by internal ADC1 channel. I configurated phy like in stm32f37x_dsp_stdperiph_lib but it dosn't works right. My code: ...

cg by Associate II
  • 1343 Views
  • 2 replies
  • 0 kudos

How fast ? ;-)

Posted on November 16, 2011 at 08:29Hello,Just wondering ... did somebody already tried to overclock an STM32 (F2 series for example) ?What max clock can we achieve before the chip blows up (with correct flash wait state) ?Thomas.

root by Associate II
  • 5177 Views
  • 14 replies
  • 0 kudos

STM32F4 ADC TIM Triggered

Posted on October 29, 2013 at 11:58 Hello, i'm trying to regulate the Samplefrequence of the ADC3 via TIM2 OC2. Case, ADC Continuous Mode = Enable: Works Case, ADC Continuous Mode = Disable: no Conversation Does anyone se...

gausa by Associate II
  • 2352 Views
  • 5 replies
  • 0 kudos

SD doubt

Posted on October 21, 2013 at 16:37Hi everyone,I have a doubt and i hope someone can help me.I'm writting my SD card files with .001, .002, .003, etc extension. I need to know which is the biggest extension of my files. I'm using Fat32. Is there any...

STM32F4 Generation PWM

Posted on October 28, 2013 at 11:06Please! Help me to generate a meander with frequency of 8 MHz on the timer - counter in mode PWM. Clocking from MCO1/MCO2 does not approach!

alem_sd by Associate II
  • 1703 Views
  • 3 replies
  • 0 kudos

Setting up SDIO interface on F4 -CMD2 issues

Posted on October 10, 2013 at 16:24Hi guys, I'm currently setting up an SD Card on the STM32F4 Discovery and have managed to so far get through the initial setup commands without too many issues. CMD0, CMD8,CMD55,CMD41 have all successfully been sen...

external interrupt issue

Posted on June 17, 2013 at 21:08 Hi there I'm pretty new to stm world I'm trying to generate an external interruption by pushing the user button on a stm32f4 discovery dev board, I tried to implement the staf via the API provided with the...

me780411 by Associate
  • 1389 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.