STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer(s) with 2 Ext inputs, one gating the other

Posted on December 12, 2013 at 06:16 I've been coding on the STM32F4 for the past couple years and love the MCU. However, I'm having trouble figuring out how to bring in two external signals and use one as the gate for the other. I'm plan...

STM32 USART interrupt problem

Posted on December 13, 2013 at 00:55My application use EXTI1 interrupt, SPI1 interrupt and USART1(RXNE) interrupt. USART1 interrupt has highest priority. USART1_IRQHandler is very short, only storing incomming bytes to the circular buffer. When I di...

ondrej2 by Associate II
  • 2739 Views
  • 5 replies
  • 0 kudos

STM32 Flash being wiped?

Posted on December 12, 2013 at 11:22Hi This is Not a software problem. This is an electrical problem! We are seeing a number of unexpected Flash sector erasures/wipes. Typically, we are powering up/down the system connecting/disconnecting USB or RS...

chen by Associate II
  • 1741 Views
  • 2 replies
  • 0 kudos

RTC Time on Discovery L152

Posted on December 06, 2013 at 08:31 Dear Sir/Madam, I am a novice ARM programmer, trying to get the hang of things. It's a bit more complex than programming an 8-bit AVR controller... Anyway I was wondering, why I cannot read th...

klemen by Associate II
  • 4662 Views
  • 11 replies
  • 0 kudos

I2C causes STM32F051 to crash/reboot

Posted on November 29, 2013 at 16:07Hello, I've an STM32F051 where i2c modules can be connected (SFP video modules) These modules should be hot swappable, however it seems that the I2C communication is not dealing properly with these modules because...

evert2 by Associate II
  • 7909 Views
  • 18 replies
  • 0 kudos

STM32F4 and ARM DS-5

Posted on December 10, 2013 at 03:34Does ARM DS-5 works with STM32F4 out of box?I downloaded one, but seems default project is linux.Thanks #what-it-says-on-the-tin #right-tool-for-the-job

sharethl by Associate II
  • 1765 Views
  • 3 replies
  • 0 kudos

Setting up HSE on STM32F4 Discovery

Posted on December 12, 2013 at 15:48 I'm sure there's probably already a post on how to do this, but I can't find it so here goes: I'm trying to set up the external 8 MHz oscillator on the F4 Discovery. I'm using Keil IDE and have set my...

USART communication via RXNE interrupt only reads one char

Posted on December 11, 2013 at 22:37Hello ST Community,I am using a STM32F2 uC for my project, and I have configured an USART interface as an UART by not initializing the clock settings. In order to program the device the UART is connected to I send...

dmg0048 by Associate II
  • 2565 Views
  • 3 replies
  • 0 kudos

Certificate Management for Embedded Devices

Posted on December 11, 2013 at 20:24One of the building blocks that we see most commonly misunderstood is how to manage SSL certificates in embedded devices. For this reason we have designed a whitepaper that provides an introduction to SSL certific...

wilfred by Associate
  • 1223 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.