STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM Studio Variables missing

Posted on January 15, 2014 at 22:55Im using STM Studio 3.3. When I import my .elf files from Keil or Coocox most of the variables (even direct variables) are missing. When I analyze the .elf file with nm or eu-nm all the variables are available on f...

werbung by Associate II
  • 1056 Views
  • 1 replies
  • 0 kudos

STM32F4Discovery and USB

Posted on January 22, 2014 at 13:16Dear All, I had a workign VCP example on STM32F4Discovery board until some recent changes to my own code (the USB and standard peripheral libraries are not changed). I use EmBlocks 1.42 IDE for compilation/debuggi...

davhak by Associate II
  • 1230 Views
  • 3 replies
  • 0 kudos

Retriggering Configured DMA for USART Tx

Posted on January 19, 2014 at 19:50Hello all,I have written a function to configure the DMA for use with one of the USARTs for TX, which works when I trigger it using DMA_Cmd() function. As with the usual USART DMA configurations, all it does is tra...

honboxuan by Associate II
  • 1318 Views
  • 1 replies
  • 0 kudos

Using Level Triggered Interrupts on STM32F4 and other devices

Posted on January 23, 2014 at 18:40Hi, All EXTI-External interrupts  on STM32Fxx and other STM32 devices implemented by STM are EDGE triggered interrupts. The ARM core however supports Level, Pulse and Edge triggered interrupts. STM32Fxx Tech.Ref.M...

canbu22 by Associate III
  • 2237 Views
  • 2 replies
  • 0 kudos

STM32F405RG using SPI2 and SPI3 at the same time with DMA?

Posted on January 23, 2014 at 16:44Hi,In my application I would like to use all three SPI interfaces of the STM32F405RG at the same time, with DMA. I noticed that SPI2 and SPI3 are both assigned to DMA1 Channel 0, but different streams. Does this me...

mluessi by Associate II
  • 1169 Views
  • 2 replies
  • 0 kudos

Deep sleep issue on STM32W108

Posted on December 27, 2013 at 11:39Hello,I am using the STM32W-RFCKIT (MB950 and MB951) to create some prototypes. I've tried both Simple MAC sample applications (sun & planets, talk) version 2.0.1 and Contiki (2.5, 2.6, 2.7). In all of these, ever...

vanja by Associate
  • 1175 Views
  • 1 replies
  • 0 kudos

STM32F103 - FSMC 8 bit BUS

Posted on January 23, 2014 at 14:24Hello,in RM008 Rev. 14 at Section 21.5.2 -''Supported memories and transactions'' -  it is written (in table 108) that memory data size is always 16 bit - can we write single byte from 8 bit BUS without effecting t...

asherp by Associate
  • 988 Views
  • 1 replies
  • 0 kudos

Forcing float on a matlab generated code

Posted on January 22, 2014 at 16:25Hi all, I use matlab to generate c code and have this code compile in IAR for STM32F4 as a library. So I have no ST libraries added just the c code and h files from matlab. Matlab uses sqrt, sin functions etc. decl...

igal by Associate II
  • 4851 Views
  • 10 replies
  • 0 kudos

I2S MCLK slew rate issue

Posted on January 22, 2014 at 20:26Hi, I've been using an audio codec with the STM32F407 Discovery. Data is transferred using I2S, with the STM32F407 as master. It generates an MCLK signal at a frequency of 256*fs, i.e at 2.048 MHz for 8 kHz samplin...

d_1 by Associate II
  • 2667 Views
  • 4 replies
  • 0 kudos

USB vendor/product ID

Posted on January 22, 2014 at 12:34Hi,I have seen mentioned in the forum that ST have provided use of their Vendor ID, with a unique Product ID to people using their processors.I would like to ask how I could obtain a unique product ID for our compa...

mark2399 by Associate II
  • 10624 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.