STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help a Hardware guy with NVIC

Posted on February 06, 2014 at 19:13I am trying to understand the NVIC on a SMT32F407. I have found that we are missing USB interrupts randomly. Since I cant solder a pullup to fix the problem I am stuck. I can understand the documentation enough to...

VE7HR by Associate II
  • 3134 Views
  • 6 replies
  • 0 kudos

Tristating GPIO as an output

Posted on February 05, 2014 at 19:19Using an STM32F407, can you have a pin set up as an output and tristated?The reason that I ask is b/c my circuit is acting like it is doing just that. With my pin configuration as follows:GPIO_InitStructure.GPIO_M...

dibs by Associate II
  • 4802 Views
  • 9 replies
  • 0 kudos

STM32F4 External Interrupts not Working

Posted on February 06, 2014 at 07:46I wrote a code to generate rising edge interrupts for a 4MHz clock input to the board. The 4MHz input is generated by MCO while the core is pushed to 168MHz. I found that certain interrupts are not being tacked at...

0690X000006050kQAA.png
sankhar by Associate
  • 1595 Views
  • 2 replies
  • 0 kudos

STM32F427 External 32 bit Dual Port Ram

Posted on February 05, 2014 at 17:20I have looked at using the STM32F427 to drive a 32 bit Universal Bus, similar to VME. I need CAN, SPI, USB etc, therefore the STM32 looks a good choice. I am finding difficulty in getting information on the FMC bu...

mp45dt02 mic passthru to DAC

Posted on December 15, 2012 at 02:25On the discovery board, the digital MEMs mic data is accessed by providing a clock from i2s_2. In the Audio_playback_record example, i2s is set up to acquire data in 16b blocks, and an interrupt (AUDIO_REC_SPI_IRQ...

davejun by Associate
  • 2488 Views
  • 6 replies
  • 0 kudos

STM32F4 discovery External interrupts not working

Posted on February 06, 2014 at 07:49I wrote a code to generate rising edge interrupts for a 4MHz clock input to the board. The 4MHz input is generated by MCO while the core is pushed to 168MHz. I found that certain interrupts are not being tacked at...

0690X00000605XEQAY.png
sankhar by Associate
  • 1334 Views
  • 2 replies
  • 0 kudos

problem with SlaveMode and interrupt

Posted on February 06, 2014 at 14:06 Hi, I need help with my Stm32F4 In this example I want to clock Tim4 with Tim2 using the slave mode. This is working fine! But when I want to use Tim4 to rise an update-interrupt this line stops the MCU. So...

STM32L152 OPAMP Output current?

Posted on February 05, 2014 at 18:41Hi All!I would like to use the  STM32L152  Opamp output pin to pulse drive the MOC3020 optotriac.The pulse current should be ca 15mA-20mA for the optotriac to fire up under any temp. conditions.Can I source this a...

Tom by Associate II
  • 1076 Views
  • 2 replies
  • 0 kudos

Vref- minimum on stm32f103

Posted on February 06, 2014 at 09:26Hello together, i´ve been searching for information about the minimal voltage wich has to applied to Vref-. In particularly it is around the stm32f103CBT6. I´ve used the search function in the RefManual, but co...

STM32F415RGT6 UART4 RXNE Interrupt ?!

Posted on May 22, 2012 at 15:25Hello, I try to work with the UART4 RXNE interrupt but something went wrong.     // USART2-TX, UART4-TX     GPIO_StructInit(&GPIO_InitStructure);     GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;     GPIO_InitStructure...

dennis23 by Associate II
  • 2376 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.